This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28069AD采样问题



今天在做28069AD采样时,给AD口一个稳定的电压(例如1V),采样到的结果总体是正确的,但是结果寄存器的值不稳定,跳动幅度最高可以达到5%。PS:用TI官方的DEMO 2806XADCS0C和火箭开发板。

  • 今天在做28069AD采样时,给AD口一个稳定的电压(例如1V),采样到�结果总体是正确的,但是结果寄存器的值不稳定,跳动幅度最高可以达到5%。PS:用TI官方的DEMO 2806XADCS0C和火箭开发板。

    Eric:

    我有点怀疑是输入信号的不稳定。如果要测ADC的精度,建议你用电池信号作为输入。

  • 你输入信号最好拿示波器看看  也即是限制带宽20MHz测试一下是不是有小于

    最小分辨率的幅度跳动    一般稳定的电压采集会有数字量的波动  但是没有你说的这么大