This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2812读数据的速度



你好!

我用2812外扩了一片AD,采样率为10MHZ,但是通过CCS观察到得数据的采样率只有1MHZ左右。

DSP与AD之间的接口为并行接口,数据映射到XINTF存储区域的地址为XINTF Zone6的0x100001。

需要采样512个数据。程序中我的设置为:

for(i=0;i<512;i++)

{

Voltage[i]=ADCDATA;  //  ADCDATA为0x100001的地址;

}

读数据时,XINTF的片选信号XZCS6引脚应该为低。但是检测到XZCS6引脚的脉冲频率为1MHZ左右。

从上面的程序中可以看到,我已经将读信号的速度设到最高了,还存在这个问题。

因此,我想请问一下,这个会是什么原因?是2812本身读信号的周期就比较长吗?

谢谢了。!

}