This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于28335中mcbsp配置成spi从机的使用接收数据不正确

Other Parts Discussed in Thread: CONTROLSUITE

在使用mcbsp进行配置成为spi的过程中,接收到的数据有错误,现在可以接收到数据,但是完全不正确,请问是什么原因,配置代码如下:

InitMcbspbGpio();
McbspaRegs.SPCR2.all=0x0000; // Reset FS generator, sample rate generator & transmitter
McbspaRegs.SPCR1.all=0x0000; // Reset Receiver, Right justify word, Digital loopback dis.
McbspaRegs.PCR.all=0x0008; //(CLKXM=CLKRM=FSXM=FSRM= 1, FSXP = 1)
McbspaRegs.SPCR1.bit.DLB = 0;
McbspaRegs.SPCR1.bit.CLKSTP = 2; // Together with CLKXP/CLKRP determines clocking scheme
McbspaRegs.PCR.bit.CLKXP = 0; // CPOL = 0, CPHA = 0 rising edge no delay
McbspaRegs.PCR.bit.CLKRP = 0;
McbspaRegs.RCR2.bit.RDATDLY=0; // FSX setup time 1 in master mode. 0 for slave mode (Receive)
McbspaRegs.XCR2.bit.XDATDLY=0; // FSX setup time 1 in master mode. 0 for slave mode (Transmit)
McbspaRegs.XCR2.bit.XPHASE=0;
McbspaRegs.RCR2.bit.RPHASE=0;
McbspaRegs.RCR1.bit.RWDLEN1=2; // 16-bit word
McbspaRegs.XCR1.bit.XWDLEN1=2; // 16-bit word
McbspaRegs.SRGR2.all=0x2000; // CLKSM=1, FPER = 1 CLKG periods
McbspaRegs.SRGR1.all= 0x0001; // Frame Width = 1 CLKG period, CLKGDV=16
McbspaRegs.SPCR2.bit.GRST=1; // Enable the sample rate generator

delay_loop(); // Wait at least 2 SRG clock cycles
McbspaRegs.SPCR2.bit.XRST=1; // Release TX from Reset
McbspaRegs.SPCR1.bit.RRST=1; // Release RX from Reset
McbspaRegs.SPCR2.bit.FRST=1;

这里有什么问题吗,采用轮询的方式来接收数据,请问有什么问题吗,现在很迷茫,因为第一次用,好多地方不懂,谢谢大家