This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2808 GPIO输出异常



 我将GPIO30连接到GPIO26,GPIO30设置为输出,GPIO26设置为输入,将GPIO30变为低时,电平为2.4V,变不成0,请问为什么?
我将GPIO30的输出,用一个3.3K的电阻上拉,还是不行
下面是GPIO30的初始化

GpioCtrlRegs.GPAPUD.bit.GPIO30 = 1; // 使能内部上拉
GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 0; // 功能 = IO
GpioCtrlRegs.GPADIR.bit.GPIO30 = 1; // 方向 = output
GpioDataRegs.GPASET.bit.GPIO30 = 1; // 更新输出缓存