This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IPCBootCPU2无法加载的问题



在F28377D中运行例程blinky时,想烧到FALSH中运行,于是在CPU1中,预先定义了_standalone和_FLASH,加载了这段代码,用来启动CPU2:IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_FLASH);

然后built的时候,出现了如下错误:

是不是仅仅在CPU1中加上这一段代码IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_FLASH);是不够的?

请问我还需要如何修改来解决这个问题呢?

麻烦各位帮忙看下,谢谢!

  • 你好,

    请问您说这段的时候:

    Dong Xu5 说:

    在F28377D中运行例程blinky时,想烧到FALSH中运行,于是在CPU1中,预先定义了_standalone和_FLASH

    是否指调整到了CPU1_FLASH_STANDALONE模式下。
    我运行相同的例程没有遇到任何问题。
    Emma
  • 你用的例程是F2837xD_examples_Cpu1文件夹下的还是F2837xD_examples_Dual文件夹下的例程,IPCBootCPU2函数是在F2837xD_Ipc_Driver_Util.c文件中定义的,前者的工程里没有添加这个.c文件