28335单步运行就进不了中断函数,但是全速运行就可以跳进去是为啥呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
28335单步运行就进不了中断函数,但是全速运行就可以跳进去是为啥呢?
您好,是SCI的FIFO中断。因事先把SCI的FIFO初始化,当把PIE和CPU中断配置好后,IFR和IER相同位便都为1,明知道下一步就是进入FIFO的发送中断,可是一直点单步运行就是不跳进去,甚至全速运行进入中断时所在主程序位置都跨过去了。最后还得是在中断程序中加断点然后全速运行才进得去。程序如下,是从例子改的,就把SCI变成free运行。
//###########################################################################
//
// FILE: Example_2833xSci_FFDLB_int.c
//
// TITLE: DSP2833x Device SCI Digital Loop Back porgram.
//
//
// ASSUMPTIONS:
//
// This program requires the DSP2833x header files.
//
// This program uses the internal loop back test mode of the peripheral.
// Other then boot mode pin configuration, no other hardware configuration
// is required.
//
// As supplied, this project is configured for "boot to SARAM"
// operation. The 2833x Boot Mode table is shown below.
// For information on configuring the boot mode of an eZdsp,
// please refer to the documentation included with the eZdsp,
//
// $Boot_Table:
//
// GPIO87 GPIO86 GPIO85 GPIO84
// XA15 XA14 XA13 XA12
// PU PU PU PU
// ==========================================
// 1 1 1 1 Jump to Flash
// 1 1 1 0 SCI-A boot
// 1 1 0 1 SPI-A boot
// 1 1 0 0 I2C-A boot
// 1 0 1 1 eCAN-A boot
// 1 0 1 0 McBSP-A boot
// 1 0 0 1 Jump to XINTF x16
// 1 0 0 0 Jump to XINTF x32
// 0 1 1 1 Jump to OTP
// 0 1 1 0 Parallel GPIO I/O boot
// 0 1 0 1 Parallel XINTF boot
// 0 1 0 0 Jump to SARAM <- "boot to SARAM"
// 0 0 1 1 Branch to check boot mode
// 0 0 1 0 Boot to flash, bypass ADC cal
// 0 0 0 1 Boot to SARAM, bypass ADC cal
// 0 0 0 0 Boot to SCI-A, bypass ADC cal
// Boot_Table_End$
//
// DESCRIPTION:
//
// This program is a SCI example that uses the internal loopback of
// the peripheral. Both interrupts and the SCI FIFOs are used.
//
// A stream of data is sent and then compared to the recieved stream.
//
// The SCI-A sent data looks like this:
// 00 01 02 03 04 05 06 07
// 01 02 03 04 05 06 07 08
// 02 03 04 05 06 07 08 09
// ....
// FE FF 00 01 02 03 04 05
// FF 00 01 02 03 04 05 06
// etc..
//
//
// The SCI-B sent data looks like this:
// FF FE FD FC FB FA F9 F8
// FE FD FC FB FA F9 F8 F7
// FD FC FB FA F9 F8 F7 F6
// ....
// 01 00 FF FE FD FC FB FA
// 00 FF FE FD FC FB FA F9
// etc..
//
// Both patterns are repeated forever.
//
// Watch Variables:
//
// SCI-A SCI-B
// ----------------------
// sdataA sdataB Data being sent
// rdataA rdataB Data received
// rdata_pointA rdata_pointB Keep track of where we are in the datastream
// This is used to check the incoming data
//###########################################################################
// Original Source by S.D.
//
// $TI Release: 2833x/2823x Header Files and Peripheral Examples V133 $
// $Release Date: June 8, 2012 $
//###########################################################################
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
#define CPU_FREQ 150E6
#define LSPCLK_FREQ CPU_FREQ/4
#define SCI_FREQ 100E3
#define SCI_PRD (LSPCLK_FREQ/(SCI_FREQ*8))-1
// Prototype statements for functions found within this file.
interrupt void sciaTxFifoIsr(void);
interrupt void sciaRxFifoIsr(void);
interrupt void scibTxFifoIsr(void);
interrupt void scibRxFifoIsr(void);
void scia_fifo_init(void);
void scib_fifo_init(void);
void error(void);
// Global variables
Uint16 sdataA[8]; // Send data for SCI-A
Uint16 sdataB[8]; // Send data for SCI-B
Uint16 rdataA[8]; // Received data for SCI-A
Uint16 rdataB[8]; // Received data for SCI-B
Uint16 rdata_pointA; // Used for checking the received data
Uint16 rdata_pointB;
void main(void)
{
Uint16 i;
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2833x_SysCtrl.c file.
InitSysCtrl();
// Step 2. Initalize GPIO:
// This example function is found in the DSP2833x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio();
// Setup only the GP I/O only for SCI-A and SCI-B functionality
// This function is found in DSP2833x_Sci.c
InitSciGpio();
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;
// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2833x_PieCtrl.c file.
InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in DSP2833x_DefaultIsr.c.
// This function is found in DSP2833x_PieVect.c.
InitPieVectTable();
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.SCIRXINTA = &sciaRxFifoIsr;
PieVectTable.SCITXINTA = &sciaTxFifoIsr;
PieVectTable.SCIRXINTB = &scibRxFifoIsr;
PieVectTable.SCITXINTB = &scibTxFifoIsr;
EDIS; // This is needed to disable write to EALLOW protected registers
// Step 4. Initialize all the Device Peripherals:
// This function is found in DSP2833x_InitPeripherals.c
// InitPeripherals(); // Not required for this example
scia_fifo_init(); // Init SCI-A
scib_fifo_init(); // Init SCI-B
// Step 5. User specific code, enable interrupts:
// Init send data. After each transmission this data
// will be updated for the next transmission
for(i = 0; i<8; i++)
{
sdataA[i] = i;
}
for(i = 0; i<8; i++)
{
sdataB[i] = 0xFF - i;
}
rdata_pointA = sdataA[0];
rdata_pointB = sdataB[0];
// Enable interrupts required for this example
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block
PieCtrlRegs.PIEIER9.bit.INTx1=1; // PIE Group 9, int1
PieCtrlRegs.PIEIER9.bit.INTx2=1; // PIE Group 9, INT2
PieCtrlRegs.PIEIER9.bit.INTx3=1; // PIE Group 9, INT3
PieCtrlRegs.PIEIER9.bit.INTx4=1; // PIE Group 9, INT4
IER = 0x100; // Enable CPU INT
ERTM;
EINT;
ERTM;
// Step 6. IDLE loop. Just sit and loop forever (optional):
for(;;);
}
void error(void)
{
asm(" ESTOP0"); // Test failed!! Stop!
for (;;);
}
interrupt void sciaTxFifoIsr(void)
{
Uint16 i;
for(i=0; i< 8; i++)
{
SciaRegs.SCITXBUF=sdataA[i]; // Send data
}
for(i=0; i< 8; i++) //Increment send data for next cycle
{
sdataA[i] = (sdataA[i]+1) & 0x00FF;
}
SciaRegs.SCIFFTX.bit.TXFFINTCLR=1; // Clear SCI Interrupt flag
PieCtrlRegs.PIEACK.bit.ACK9=1;
}
interrupt void sciaRxFifoIsr(void)
{
Uint16 i;
for(i=0;i<8;i++)
{
rdataA[i]=SciaRegs.SCIRXBUF.all; // Read data
}
for(i=0;i<8;i++) // Check received data
{
if(rdataA[i] != ( (rdata_pointA+i) & 0x00FF) ) error();
}
rdata_pointA = (rdata_pointA+1) & 0x00FF;
SciaRegs.SCIFFRX.bit.RXFFOVRCLR=1; // Clear Overflow flag
SciaRegs.SCIFFRX.bit.RXFFINTCLR=1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.bit.ACK9=1; // Issue PIE ack
}
void scia_fifo_init()
{
SciaRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
SciaRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
SciaRegs.SCICTL2.bit.TXINTENA =1;
SciaRegs.SCICTL2.bit.RXBKINTENA =1;
SciaRegs.SCIHBAUD =0x0001; // 9600 baud @LSPCLK = 37.5MHz.
SciaRegs.SCILBAUD =0x00E7;
// SciaRegs.SCIHBAUD = 0x0000;
// SciaRegs.SCILBAUD = SCI_PRD;
SciaRegs.SCICCR.bit.LOOPBKENA =1; // Enable loop back
SciaRegs.SCIFFTX.all=0xC028;
SciaRegs.SCIFFRX.all=0x0028;
SciaRegs.SCIFFCT.all=0x00;
SciaRegs.SCIPRI.bit.FREE=1;
SciaRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
SciaRegs.SCIFFTX.bit.TXFIFOXRESET=1;
SciaRegs.SCIFFRX.bit.RXFIFORESET=1;
}
interrupt void scibTxFifoIsr(void)
{
Uint16 i;
for(i=0; i< 8; i++)
{
ScibRegs.SCITXBUF=sdataB[i]; // Send data
}
for(i=0; i< 8; i++) //Increment send data for next cycle
{
sdataB[i] = (sdataB[i]-1) & 0x00FF;
}
ScibRegs.SCIFFTX.bit.TXFFINTCLR=1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.all|=0x100; // Issue PIE ACK
}
interrupt void scibRxFifoIsr(void)
{
Uint16 i;
for(i=0;i<8;i++)
{
rdataB[i]=ScibRegs.SCIRXBUF.all; // Read data
}
for(i=0;i<8;i++) // Check received data
{
if(rdataB[i] != ( (rdata_pointB-i) & 0x00FF) ) error();
}
rdata_pointB = (rdata_pointB-1) & 0x00FF;
ScibRegs.SCIFFRX.bit.RXFFOVRCLR=1; // Clear Overflow flag
ScibRegs.SCIFFRX.bit.RXFFINTCLR=1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.all|=0x100; // Issue PIE ack
}
void scib_fifo_init()
{
ScibRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
ScibRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
ScibRegs.SCICTL2.bit.TXINTENA =1;
ScibRegs.SCICTL2.bit.RXBKINTENA =1;
ScibRegs.SCIHBAUD =0x0000;
ScibRegs.SCILBAUD =SCI_PRD;
ScibRegs.SCICCR.bit.LOOPBKENA =1; // Enable loop back
ScibRegs.SCIFFTX.all=0xC028;
ScibRegs.SCIFFRX.all=0x0028;
ScibRegs.SCIFFCT.all=0x00;
ScibRegs.SCIPRI.bit.FREE=1;
ScibRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
ScibRegs.SCIFFTX.bit.TXFIFOXRESET=1;
ScibRegs.SCIFFRX.bit.RXFIFORESET=1;
}
//===========================================================================
// No more.
//===========================================================================