This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

有C28X控制的DC-DC或者DC-AC开发板吗?



要求DC输出50V1A小功率的,如果有想买个学习一下

  • TI 官网上有一套 C2000 Low-Voltage Solar Explorer Kit

    包括DC/DC和DC/AC,输出功率50W。

    Features

    20VDC/ 50W Non Isolated Design

    Built-in panel emulator

    Single switch DC/DC Boost for Maximum Power Point Tracking

    DC/DC SEPIC for MPPT and Battery Charging

    36VDC Intermediary bus

    24VAC Output Inverter stage

    Isolated USB JTAG built-in

    PN:TMDSSOLARPEXPKIT