This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000 28377的ADC16位差分ADC如何使用



C2000 28377的ADC16位差分ADC如何使用?

在手册上看到ADCINA0为正,ADCINA1为负,且不能通过将负输入ADCINA1连接到VSSA或VREFLO?这句话是什么意思?我的是普通的放大器,单端输出,如何接到ADCINA0,ADCINA1,ADCINA1不能直接接到VSSA吗?看到手册里ADCINA0,ADCINA1对VSSA电压应该为VREFHI + VREFLO)/2,这个怎么实现?如果我的VREFHI =3V,ADCINA0对VSSA需要为1.5V,ADCINA1对VSSA也需要为1.5V?

期待回复,谢谢