This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28075  SPI普通模式时最大波特率为lspclk/4,那配置为高速模式有什么用呢



28075  SPI普通模式时最大波特率为lspclk/4,那配置为高速模式有什么用呢

  • 高速模式应该是针对硬件讲的 比如配置为高速模式后 IO口的翻转速度可以更高
    但是可能会增大功耗 没有必要的时候配置为低速模式
  • 您好,
    请参考手册17.3.9 SPI High-Speed Mode详细描述。
    The SPI module is capable of reaching full-duplex communication speeds up to LSPCLK/4 (where
    LSPCLK equals SYSCLK). For the maximum rated speed, refer the device Data Manual.
    In order to achieve the maximum full-duplex speeds, two restrictions are placed on the design:
    • High-speed capability is available on a single pin mux option
    • Single master to single slave configuration is supported to limit the loading on the pins.
    When configuring the GPIOs to support High-Speed mode, refer to GPIOs Required for High-Speed Mode
    for more information.