This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问大神们:28377D能否外接nand flash,其中flash的CLE和ALE如何连



请问大神们:28377D能否外接nand flash,其中flash的CLE和ALE如何连

  • 您好,
    F28377d不支持外接nand flash。
    详细请见手册:
    25.1.1 Purpose of the Peripheral
    This EMIF memory controller is compliant with the JESD21-C SDR SDRAM memories utilizing a 32-bit/16-bit data bus. The purpose of this EMIF is to provide a means for the CPU to connect to a variety of external devices including:
    • Single data rate (SDR) SDRAM
    • Asynchronous devices including NOR Flash and SRAM
    A common use for the EMIF is to interface with both a flash device and an SDRAM device simultaneously.
    Section 25.4 contains an example of operating the EMIF in this configuration.
  • 谢谢您的解答

    1、我找到了下面一个文档,能否把EMIF的两根地址线作为NAND FLASH的CLE和ALE,通过变化地址访问NAND FLASH?

    http://blog.csdn.net/zengaliang/article/details/78787331

    2、我想在EMIF1上同时扩展SDRAM和SRAM,发现SRAM的高位地址和SDRAM的CAS、RAS等控制线复用了,如EM1_A13/EM1CAS,EM1_A14/EM1RAS

    EM1_A15/EM1DQM0等。SDRAM和SRAM能否同时扩展呢,或者我在程序中实时设置管脚映射功能?

    谢谢