This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我是刚学习这个例程的,level1已经测试过了。level2有点问题希望大神能帮忙指导一下:
1、level2阶段中先测量了A相和B相的电流,这个是用内部自带的AD吗?
2、既然测量了A、B两相的电流,并且做了3/2变换和2s/2r变换,那么接下来的2r/2s变换的D、Q轴参数不是可以用2s/2r的输出结果么?然而程序里用的还是VdTesting和VqTesting。是不是因为没有经过PID这个环节?
3、该阶段也对电压进行了测量和计算,但是只作为DLOG绘图使用,这个量还有其他用途么?
学生党,手头并无相关的套件,理解起来有点困难恳请大神能解释一下相关的level调试步骤,感激不尽!