This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccs6.1linkmatlab2013a 出现以下问题



 The call to idelink_ert_make_rtw_hook, during the exit hook generated the following error:
Error while building the project.

The build process will terminate as a result.

Caused by:
Error while building the project.
The build failed with the following message: "D:/ti/ccsv6/tools/compiler/c2000_6.2.7/bin/cl2000" -I"D:/matlab2013a/toolbox/idelink/extensions/ticcs/inc" -I"D:/matlab2013a/LED_F28335_SM_ticcs" -I"D:/matlab2013a" -I"C:/Users/longyong/Desktop" -I"D:/matlab2013a/extern/include" -I"D:/matlab2013a/simulink/include" -I"D:/matlab2013a/rtw/cc" -I"D:/matlab2013a/rtw/cc/ext_mode/common" -I"D:/matlab2013a/rtw/c/ert" -D"__TICCSC__" -D"RT" -D"USE_RTMODEL" -ml -v28 --float_support=fpu32 -D"MODEL=LED_F28335_SM" -D"NUMST=1" -D"NCSTATES=0" -D"HAVESTDIO=" -D"ONESTEPFCN=1" -D"TERMFCN=1" -D"MAT_FILE=0" -D"MULTI_INSTANCE_CODE=0" -D"INTEGER_CODE=0" -D"MT=0" -D"CLASSIC_INTERFACE=0" -D"TID01EQ=0" -I"D:\ti\ccsv6\tools\compiler\c2000_6.2.7\include" -fr"./derived/" ./LED_F28335_SM.c ./LED_F28335_SM_main.c ./MW_c28xx_board.c ./MW_c28xx_csl.c ./DSP2833x_ADC_cal.asm ./DSP2833x_CodeStartBranch.asm ./DSP2833x_CpuTimers.c ./DSP2833x_DMA.c ./DSP2833x_DefaultIsr.c ./DSP2833x_GlobalVariableDefs.c ./DSP2833x_MemCopy.c ./DSP2833x_PieCtrl.c ./DSP2833x_PieVect.c ./DSP2833x_SysCtrl.c ./DSP2833x_usDelay.asm
[LED_F28335_SM.c]
[LED_F28335_SM_main.c]
[MW_c28xx_board.c]
[MW_c28xx_csl.c]
[DSP2833x_ADC_cal.asm]
[DSP2833x_CodeStartBranch.asm]
[DSP2833x_CpuTimers.c]
[DSP2833x_DMA.c]
[DSP2833x_DefaultIsr.c]
[DSP2833x_GlobalVariableDefs.c]
[DSP2833x_MemCopy.c]
[DSP2833x_PieCtrl.c]
[DSP2833x_PieVect.c]
[DSP2833x_SysCtrl.c]
[DSP2833x_usDelay.asm]
"D:/ti/ccsv6/tools/compiler/c2000_6.2.7/bin/cl2000" -z -l"rts2800_fpu32.lib" -c -x -m"LED_F28335_SM.map" -stack0x200 -I"D:\ti\ccsv6\tools\compiler\c2000_6.2.7\lib" -o ./CustomMW/LED_F28335_SM.out ./derived/LED_F28335_SM.obj ./derived/LED_F28335_SM_main.obj ./derived/MW_c28xx_board.obj ./derived/MW_c28xx_csl.obj ./derived/DSP2833x_ADC_cal.obj ./derived/DSP2833x_CodeStartBranch.obj ./derived/DSP2833x_CpuTimers.obj ./derived/DSP2833x_DMA.obj ./derived/DSP2833x_DefaultIsr.obj ./derived/DSP2833x_GlobalVariableDefs.obj ./derived/DSP2833x_MemCopy.obj ./derived/DSP2833x_PieCtrl.obj ./derived/DSP2833x_PieVect.obj ./derived/DSP2833x_SysCtrl.obj ./derived/DSP2833x_usDelay.obj ./LED_F28335_SM.cmd ../toolbox/idelink/extensions/ticcs/rtlib/IQmath_fpu32.lib
<Linking>
error: cannot find file "rts2800_fpu32.lib"
error: errors encountered during linking; "./CustomMW/LED_F28335_SM.out" not
built

>> Compilation failure