我第一次使用28379D的芯片,在调试CLA时遇到了麻烦,希望能得到大家的帮助:
我使用汇编语言编写程序,在DUG模式下,CLA可以正常运行,一旦将芯片复位,就不能重新启动运行。
我怎么配置CMD文件才能使CLA的程序能从FLASH自动加载到RAM区,并自动运行?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我第一次使用28379D的芯片,在调试CLA时遇到了麻烦,希望能得到大家的帮助:
我使用汇编语言编写程序,在DUG模式下,CLA可以正常运行,一旦将芯片复位,就不能重新启动运行。
我怎么配置CMD文件才能使CLA的程序能从FLASH自动加载到RAM区,并自动运行?
因为,我们的整个工程是用汇编语言构成的,所以我们的CMD文件也是自己配置的,我现在是不知道我的CMD文件那里出错了,导致CLA程序不能载入到FLASH中?以下是我们的CMD文件,能否请您帮忙诊断一下?
MEMORY
{
PAGE 0 : /* Program Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
/* BEGIN is used for the "boot to Flash" bootloader mode */
BEGIN : origin = 0x80000, length = 0x000002
// RAMM0 : origin = 0x000122, length = 0x0002DE
// RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
// RAMGS14 : origin = 0x01A000, length = 0x001000
// RAMGS15 : origin = 0x01B000, length = 0x001000
RESET : origin = 0x3FFFC0, length = 0x000002
/* Flash sectors */
FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASHB : origin = 0x082000, length = 0x001000 /* on-chip Flash */
FLASHB_1 : origin = 0x083000, length = 0x001000 /* on-chip Flash */
FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */
FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */
FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASHN : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */
BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMD1 : origin = 0x00B800, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMGS0 : origin = 0x00C000, length = 0x001000
RAMGS1 : origin = 0x00D000, length = 0x001000
RAMGS2 : origin = 0x00E000, length = 0x001000
RAMGS3 : origin = 0x00F000, length = 0x001000
RAMGS4 : origin = 0x010000, length = 0x001000
RAMGS5 : origin = 0x011000, length = 0x001000
RAMGS6 : origin = 0x012000, length = 0x001000
RAMGS7 : origin = 0x013000, length = 0x001000
RAMGS8 : origin = 0x014000, length = 0x001000
RAMGS9 : origin = 0x015000, length = 0x001000
RAMGS10 : origin = 0x016000, length = 0x001000
RAMGS11 : origin = 0x017000, length = 0x001000
RAMGS12 : origin = 0x018000, length = 0x001000
RAMGS13 : origin = 0x019000, length = 0x001000
CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400
CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400
}
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHB PAGE = 0, ALIGN(4)
.pinit : > FLASHB, PAGE = 0, ALIGN(4)
.text : >> FLASHB | FLASHC | FLASHD | FLASHE PAGE = 0, ALIGN(4)
// claprog : >> RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3 |RAMLS4 PAGE = 0, ALIGN(4)
ClaProg : LOAD = FLASHB_1,
RUN = RAMLS0,
LOAD_START(_Cla1funcsLoadStart),
LOAD_END(_Cla1funcsLoadEnd),
RUN_START(_Cla1funcsRunStart),
LOAD_SIZE(_Cla1funcsLoadSize),
PAGE = 0, ALIGN(4)
// CLADataLS0 : > RAMLS0, PAGE=1
// CLADataLS1 : > RAMLS1, PAGE=1
// Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1
// CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1
.stack : > RAMM1 PAGE = 1
.ebss : >> RAMLS5 | RAMGS0 | RAMGS1 PAGE = 1
.esysmem : > RAMLS5 PAGE = 1
/* Initalized sections go in Flash */
// .econst : >> FLASHF | FLASHG | FLASHH PAGE = 0, ALIGN(4)
// .switch : > FLASHB PAGE = 0, ALIGN(4)
_c_int00 : > FLASHA PAGE = 0
wd_disable : > FLASHA PAGE = 0
codestart : > BEGIN, PAGE = 0
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
/* 。const_cla : LOAD = FLASHB,
RUN = RAMLS0,
RUN_START(_Cla1ConstRunStart),
LOAD_START(_Cla1ConstLoadStart),
LOAD_SIZE(_Cla1ConstLoadSize),
PAGE = 1
*/
}
我用2837xD_FLASH_CLA_lnk_cpu1.cmd代替了我的CMD文件,CLA的程序照样不能烧录到FLASH中,可能会是什么问题导致的?以下是我的整个工程,请您帮忙诊断一下,为盼!谢谢
“
我用2837xD_FLASH_CLA_lnk_cpu1.cmd代替了我的CMD文件,CLA的程序照样不能烧录到FLASH中,可能会是什么问题导致的?以下是我的整个工程,请您帮忙诊断一下,为盼!谢谢
”
Eric:
||pwrite *xar7, *xar6++
prgrldrt: lret
;.text
.sect "ClaProg"
;任务1,由定时器1触发
cla1isr1: mmov32 mr0,@0xa820
这个要改成大写的ClaProg, 和cmd定义一致,
ClaProg : LOAD = FLASHD,
RUN = RAMLS0,
LOAD_START(_Cla1funcsLoadStart),
LOAD_END(_Cla1funcsLoadEnd),
RUN_START(_Cla1funcsRunStart),
LOAD_SIZE(_Cla1funcsLoadSize),
PAGE = 0, ALIGN(4)