This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Vloop 關於 BLPFC

Other Parts Discussed in Thread: CONTROLSUITE

当我将Build3用于我的BLPFC板时。

输出电压达到310V,TI程序的PWM将截止。

我认为输出电压在三个串联电阻上分为1M,1M和22K,而输出电压达到310V,这已经超过VBUS_OVP_THRSHLD((int32)((440.0 / VBUS_FULL_RANGE)* 4096 * 4096))

我能做些什么来解决这个问题,或者TI做什么来解决这个问题

SCH来自controlSUITE \ development_kits \ BLPFC_v1.0 \ Hardware
该软件来自controlSUITE \ development_kits \ BLPFC_v1.0