各位好,今天使用F28035的SCIa通讯,一直出现乱码。电路板的晶振的6M,程序是从官网例程里面拷贝的。
使用官网的例程数据正常,把程序复制到我原来的程序里面,根据6M的晶振设置波特率9600之后,一直是乱码。
下面是程序:
1、时钟配置_6M
系统时钟:
//#define DSP28_DIVSEL 0 // Enable /4 for SYSCLKOUT
#define DSP28_DIVSEL 1 // Disable /4 for SYSCKOUT
//#define DSP28_DIVSEL 2 // Enable /2 for SYSCLKOUT
//#define DSP28_DIVSEL 3 // Enable /1 for SYSCLKOUT
//#define DSP28_PLLCR 12 // Uncomment for 60 MHz devices [60 MHz = (10MHz * 12)/2]
//#define DSP28_PLLCR 11
#define DSP28_PLLCR 10
//#define DSP28_PLLCR 9
外设时钟:
//GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 3; // GPIO18 = XCLKOUT
SysCtrlRegs.LOSPCP.all = 0x0002;
// XCLKOUT to SYSCLKOUT ratio. By default XCLKOUT = 1/4 SYSCLKOUT
//XCLKOUT与SYSCLKOUT的比例。 默认情况下,XCLKOUT = 1/4 SYSCLKOUT
SysCtrlRegs.XCLK.bit.XCLKOUTDIV=2;
2、SCI设置
参数:
void scia_echoback_init()
{
// Note: Clocks were turned on to the SCIA peripheral
// in the InitSysCtrl() function
SciaRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
SciaRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
//SciaRegs.SCICTL2.bit.TXINTENA =1;
//SciaRegs.SCICTL2.bit.RXBKINTENA =1;
SciaRegs.SCIHBAUD =0x0000; // 9600 baud @LSPCLK = 15MHz (60 MHz SYSCLK).
SciaRegs.SCILBAUD =0x00C2;
SciaRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
}
引脚:
void InitSciaGpio()
{
EALLOW;
/* Enable internal pull-up for the selected pins */
// Pull-ups can be enabled or disabled disabled by the user.
// This will enable the pullups for the specified pins.
GpioCtrlRegs.GPAPUD.bit.GPIO28 = 0; // Enable pull-up for GPIO28 (SCIRXDA)
// GpioCtrlRegs.GPAPUD.bit.GPIO7 = 0; // Enable pull-up for GPIO7 (SCIRXDA)
GpioCtrlRegs.GPAPUD.bit.GPIO29 = 0; // Enable pull-up for GPIO29 (SCITXDA)
// GpioCtrlRegs.GPAPUD.bit.GPIO12 = 0; // Enable pull-up for GPIO12 (SCITXDA)
/* Set qualification for selected pins to asynch only */
// Inputs are synchronized to SYSCLKOUT by default.
// This will select asynch (no qualification) for the selected pins.
GpioCtrlRegs.GPAQSEL2.bit.GPIO28 = 3; // Asynch input GPIO28 (SCIRXDA)
// GpioCtrlRegs.GPAQSEL1.bit.GPIO7 = 3; // Asynch input GPIO7 (SCIRXDA)
/* Configure SCI-A pins using GPIO regs*/
// This specifies which of the possible GPIO pins will be SCI functional pins.
GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 1; // Configure GPIO28 for SCIRXDA operation
// GpioCtrlRegs.GPAMUX1.bit.GPIO7 = 2; // Configure GPIO7 for SCIRXDA operation
GpioCtrlRegs.GPAMUX2.bit.GPIO29 = 1; // Configure GPIO29 for SCITXDA operation
// GpioCtrlRegs.GPAMUX1.bit.GPIO12 = 2; // Configure GPIO12 for SCITXDA operation
EDIS;
}
其他的程序都是跟官网一样。
正常数据:
Hello World!
You will enter a character, and the DSP will echo it back!
Enter a character: You sent: l
Enter a character:
乱码:
?
卫?
0
0鹞
鹞
>
俐
?0
0
请教各位,多谢!