This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28027不控制XRS脚可以SCI下载程序?



感谢的解答:

e2echina.ti.com/.../151958

改正了VDD的接法后,我用PC的232接口的DTR信号驱动一个三极管OC输出接XRS脚,同时用PC的232接口的RTS信号驱动一个三极管OC输出接22脚,打开C2Prog企图下载程序,但提示无响应;手动测试过DTR有效时XRS会被拉低,RTS有效时22脚也会被拉低。然后我试一下断开了XRS脚与外部的连接,竟然能成功下载程序了!这好像不对啊?为什么不控制XRS能下载程序呢?是什么回事呢?

另外,下载的程序不能预期运行:这个程序是用 C2000Ware_1_00_03_00\device_support\f2802x\examples\structs\timed_led_blink 改了其中的GPIO34为GPIO36(21脚),3.3V经430欧电阻串一个发光二极管接至21脚,这个发光二极管未能按预期闪亮,... ...