对于2812的ad转换的精度,应怎样进行修正?能让精度达到多少?因为实际测量中感觉只靠ad转换误差较大,能看到转换的最后3位都是在变化的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
对于2812的ad转换的精度,应怎样进行修正?能让精度达到多少?因为实际测量中感觉只靠ad转换误差较大,能看到转换的最后3位都是在变化的。
TI网上有专门的文档介绍校准 AD 的方法,而且还有相应的程序,你可以去下载 。我这里发的是61ic上面的相关资料:
F2812片内AD校准代码(可以轻松将片内ADC精度校准到3%)
www.61ic.com/.../viewthread.php
怎么提高TMSF2812片上AD的精度
您好!
F2812如果不做外部硬件校正或者内部软件校正的话,正常情况下的ENOB为8~9位,如果是9位的话,即损失了12-9=3位,即有2的3次方=8个数在跳,例如2012~2010在这样的范围内跳动。
如果想有更好的精度需要校正,关于校正,TI已经给出历程,详见检索号:spra989a, 其中有说明文档和历程。F281x ADC calibration.
您好!我下载了官方的pmsm3.1的例程,可建立完工程后,出现了
"C:/ti/DMC/v32x/sys/PMSM3_4_281x/cIQmath/include/target.h", line 39: fatal error: #error Critical: A target must be defined Please define a target in the CCS Build Options/Compiler Tab/Preprocessor/ Symbol defines.
我不知道是什么原因?您能帮我解答吗