This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[28335]经常出现low-power mode错误



硬件:电压3.3V供电正常,内核电压1.9到2V之间;XRS高电平;仿真器XDS100V3;

现象:debug运行到InitXintf16Gpio();就会出现low-power mode,然后就自动退出debug;

想请教:该如何解决?

  • 可能供电电压被拉下来了,”debug运行到InitXintf16Gpio();就会出现low-power mode“ 用示波器看一下电压
  • 您的电路板是自己设计的还是TI的?
    试下用TI的例程调试是否也会出现这个问题。
  • 自己设计的,用别的开发板没有这个问题

  • DSP供电电压3.3~3.5V之间,内核电压1.9~2.0之间,都正常的额
  • 主要看瞬间跌落。
  • 没有跌落。。
  • 当我把以下代码注释掉后,就好了。

    Uint16 *ExSRAM_TEST = (Uint16 *)0x100000;

    *ExSRAM_TEST = 10;

    cc = *ExSRAM_TEST;

    我现在对xintf的硬件配置如下:

    cmd文件如下

    MEMORY
    {
    PAGE 0 :
    /* BEGIN is used for the "boot to SARAM" bootloader mode */

    BEGIN : origin = 0x000000, length = 0x000002 /* Boot to M0 will go here */
    RAMM0 : origin = 0x000050, length = 0x0003B0
    RAML0 : origin = 0x008000, length = 0x001000
    RAML1 : origin = 0x009000, length = 0x003000
    // RAML2 : origin = 0x00A000, length = 0x001000
    // RAML3 : origin = 0x00B000, length = 0x001000
    ZONE6 : origin = 0x100000, length = 0x080000
    ZONE7A : origin = 0x200000, length = 0x00FC00 /* XINTF zone 7 - program space */
    CSM_RSVD : origin = 0x33FF80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
    CSM_PWL : origin = 0x33FFF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
    ADC_CAL : origin = 0x380080, length = 0x000009
    RESET : origin = 0x3FFFC0, length = 0x000002
    IQTABLES : origin = 0x3FE000, length = 0x000b50
    IQTABLES2 : origin = 0x3FEB50, length = 0x00008c
    FPUTABLES : origin = 0x3FEBDC, length = 0x0006A0
    BOOTROM : origin = 0x3FF27C, length = 0x000D44


    PAGE 1 :
    /* BOOT_RSVD is used by the boot ROM for stack. */
    /* This section is only reserved to keep the BOOT ROM from */
    /* corrupting this area during the debug process */

    BOOT_RSVD : origin = 0x000002, length = 0x00004E /* Part of M0, BOOT rom will use this for stack */
    RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
    RAML4 : origin = 0x00C000, length = 0x001000
    RAML5 : origin = 0x00D000, length = 0x001000
    RAML6 : origin = 0x00E000, length = 0x001000
    RAML7 : origin = 0x00F000, length = 0x001000
    ZONE7B : origin = 0x20FC00, length = 0x000400 /* XINTF zone 7 - data space */
    }

    我想完成的是往sram里写个数据,然后再读出来。

    目前一旦把那三行代码加上就出错,去掉就不会。。想请教该怎么做?