This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROJ_LAB05b 起动过流保护



现使用28027F芯片,电机功率1.5KW, AC380V供电,电机30对极,最高转速500转。

现像1.使用Lab1b在AC220V或者380V供电开环起动可以运行,可以初步判断硬件没有问题。

         2.在使用Lab5b时,在220V供电时,可以起动,但起动电流偏大,存大抖动。可以正常起来,但是在AC380V时,PWM输出10MS左右,就报过流。

问题:1,为什么使用Lab1开环可以起动,Lab5B起动不了?

         2. 在Lab5B里面可以使用开环起动吗?如何开环起动电流,开环频率,开环动作时间?