你好,我是参加TI在珠海的研讨会时幸运地获得了Piccolo F2806x controlstrick 开发工具的。
我是名初学者。
问题一是:
在我使用CCS V.5编译例程2806x CLA(就是研讨会工程师示例那个,一共有三个)总是出现一个错误和两个警告,错误显示为:“Could not open the editor: C:\Documents and Settings\a0219092\user\CCSTargetConfigurations\28069.ccxml (系统找不到指定的路径。)”。我不知道怎么处理,
问题二:
还有就是在导入这个例程的最后一步是configuration target file。光盘里有这个过程演示,但是我实际操作时,在save the configuration之后下面那个test connection就亮了,点了之后出现
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\ADMINI~1\AppData\Local\.TI\2371342587\ 0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product. This utility will load the adapter 'jioserdesusb.dll'.
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-151' (0xffffff69). The title is 'SC_ERR_FTDI_OPEN'.
The explanation is: One of the FTDI driver functions used during the connect returned bad status or an error. The cause may one or more of: invalid emulator serial number, blank emulator EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the emulator can be located.
[End]
我也不知道下一步该做什么,如何才能进行debug。
问题三:
那根黑色的线如何正确插在开发板的引脚上开发板。
谢谢回答