你好!
怎么在技术论坛里面不能回复啊?下面是你提的问题:
楼主是每次都碰到这个问题,还是偶尔碰到?问题出现后芯片还可以再次烧写吗? 楼主用的是下面目录里的例程吗? C:\TI\controlSUITE\libs\utilities\flash_api\2833x\28335\v210\example_ccsv4
每次烧写都是这样的,出现问题后能成功察除,成功下载,但每次都认证不了,然后CCS3.3就报错,我用的就是这个例程。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
怎么在技术论坛里面不能回复啊?下面是你提的问题:
楼主是每次都碰到这个问题,还是偶尔碰到?问题出现后芯片还可以再次烧写吗? 楼主用的是下面目录里的例程吗? C:\TI\controlSUITE\libs\utilities\flash_api\2833x\28335\v210\example_ccsv4
每次烧写都是这样的,出现问题后能成功察除,成功下载,但每次都认证不了,然后CCS3.3就报错,我用的就是这个例程。
Trouble Setting Breakpoint with the Action...这类报错,可以做请做下面几件事情,然后重新编译程序,重新导入试试是否还会发生:
1、在CCS-->Debug => Breakpoint 选择remove all breakpoint
2、Option => Customize => Program/Project Load => Disable All Breakpoint
3、Option->Customiz->Program/Project/CIO -->Do not set CIO breakpoint at load."和"Do not set end of program breakpoint at load
另外CCSV3已经被淘汰,建议考虑用CCSV5: