This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CAL中使用const数据的问题请教!



在CLA程序中,需要使用const   short   Table[] = {0,1,2...},CMD的CLA部分定义如下:

CLAscratch       :
                     { *.obj(CLAscratch)
                     . += CLA_SCRATCHPAD_SIZE;
                     *.obj(CLAscratch_end) } >  RAMLS0,  PAGE = 1

   .scratchpad      : > RAMLS0,       PAGE = 1
   .bss_cla         : > RAMLS0,       PAGE = 1
   .const_cla       :  LOAD = FLASHB,
                       RUN = RAMLS0,
                       RUN_START(_Cla1ConstRunStart),
                       LOAD_START(_Cla1ConstLoadStart),
                       LOAD_SIZE(_Cla1ConstLoadSize),
                       PAGE = 1

程序编译后出现下面报警:

"../FLASH_lnk_cpu1.cmd", line 274: error #10265: no valid memory range(NULL) available for placement of ".const_cla"
"../FLASH_lnk_cpu1.cmd", line 274: error #10099-D: program will not fit into available memory.  load placement with alignment/blocking fails for section ".const_cla" size 0x20 page 1

变量Cla1ConstRunStart、Cla1ConstLoadStart、Cla1ConstLoadSize也没有看到在哪里定义,例程中也没有发现哪里用const数据的;

盼复!!!