This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28069_ADC初始化設定詢問_使用EPWM1中斷MAINISR



各位前輩大家好
小弟目前使用F28069,SVPWM驅動三相馬達
為了要讀取電流會授做閉迴路控制,使用ADC

主程式架構 參考了PM_Sensorless 
使用EPWM1當做MAINISR,內容與 PM_Sensorless LEVEL2 相同
而ADC初始化設定 使用 F2806XILEG_VDC_PM.H 的 ADC_MACRO()

但當我ENABLEFLAG  =1 時 中斷無法進行 CCS DEBUG 跳到 F2806x_DefaultIsr.c 的  ILLEGAL_ISR(void) 
下列為我相關的設定,想請問我 哪裡設定錯誤 或者 遺漏了甚麼
非常感謝

void main(void)

{.......

   InitSysCtrl();

   InitPieCtrl();

   InitPieVectTable();

    EALLOW;

   SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;

   EDIS;

   .....

   ADC_MACRO() 

   .....

    EALLOW;

    SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;

   EDIS;

   EALLOW;  // This is needed to write to EALLOW protected registers

   PieVectTable.EPWM1_INT = &MainISR;

   EDIS;    // This is needed to disable write to EALLOW protected registers

   PieCtrlRegs.PIEIER3.bit.INTx1 = 1;

   EPwm1Regs.ETSEL.bit.INTEN = 1;   // Enable EPWM1INT generation

   EPwm1Regs.ETSEL.bit.INTSEL = 1;  // Enable interrupt CNT_zero event

   EPwm1Regs.ETPS.bit.INTPRD = 1;   // Generate interrupt on the 1st event

   EPwm1Regs.ETCLR.bit.INT = 1;     // Enable more interrupts   //20180517!!

 

   IER |= M_INT3;

:

   EINT;   // Enable Global interrupt INTM

   ERTM;   // Enable Global realtime interrupt DBGM

....

}  //end main

上為主程式

interrupt void MainISR(void)

{

    if(EnableFlag == 1)

    {   

  ........

   EPwm1Regs.ETCLR.bit.INT = 1;

   // Acknowledge this interrupt to receive more interrupts from group 3

   PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;

    }//end enableflag =1

}//end main_isr

上為中斷

下為ADC設定

#define ADC_MACRO() \

\

 DELAY_US(ADC_usDELAY); \

    AdcRegs.ADCCTL1.all=ADC_RESET_FLAG; \

asm(" NOP "); \

asm(" NOP ");    \

\

EALLOW; \

AdcRegs.ADCCTL1.bit.ADCBGPWD = 1; /* Power up band gap */ \

\

DELAY_US(ADC_usDELAY); /* Delay before powering up rest of ADC */ \

\

AdcRegs.ADCCTL1.bit.ADCREFSEL = 0; \

    AdcRegs.ADCCTL1.bit.ADCREFPWD = 1; /* Power up reference */ \

    AdcRegs.ADCCTL1.bit.ADCPWDN = 1; /* Power up rest of ADC */ \

AdcRegs.ADCCTL1.bit.ADCENABLE = 1; /* Enable ADC */ \

\

asm(" RPT#100 || NOP"); \

\

AdcRegs.ADCCTL1.bit.INTPULSEPOS=1; \

AdcRegs.ADCCTL1.bit.TEMPCONV=0; \

\

DELAY_US(ADC_usDELAY); \

\

/******* CHANNEL SELECT *******/ \

\

\

AdcRegs.ADCSOC0CTL.bit.CHSEL = 1;    /* ChSelect: ADC A1-> Phase U Churrent*/ \

AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 5; /* Set SOC0 start trigger on EPWM1A, due to round-robin SOC0 converts first then SOC1*/ \

AdcRegs.ADCSOC0CTL.bit.ACQPS = 6; /* Set SOC0 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)*/ \

\

AdcRegs.ADCSOC1CTL.bit.CHSEL = 9; /* ChSelect: ADC B1-> Phase V Current*/ \

AdcRegs.ADCSOC1CTL.bit.TRIGSEL  = 5; \

AdcRegs.ADCSOC1CTL.bit.ACQPS = 6; \

\

AdcRegs.ADCSOC2CTL.bit.CHSEL = 10; /* ChSelect: ADC B2-> DC Bus Voltage*/ \

AdcRegs.ADCSOC2CTL.bit.TRIGSEL  = 5; \

AdcRegs.ADCSOC2CTL.bit.ACQPS = 6; \

\

AdcRegs.ADCSOC3CTL.bit.CHSEL = 15; /* ChSelect: ADC B7-> V Phase A */ \

AdcRegs.ADCSOC3CTL.bit.TRIGSEL = 5; \

AdcRegs.ADCSOC3CTL.bit.ACQPS = 6; \

\

AdcRegs.ADCSOC4CTL.bit.CHSEL = 7; /* ChSelect: ADC A7-> V Phase B */ \

AdcRegs.ADCSOC4CTL.bit.TRIGSEL  = 5; \

AdcRegs.ADCSOC4CTL.bit.ACQPS = 6; \

\

AdcRegs.ADCSOC5CTL.bit.CHSEL = 12; /* ChSelect: ADC B4-> V Phase C */ \

AdcRegs.ADCSOC5CTL.bit.TRIGSEL  = 5; \

AdcRegs.ADCSOC5CTL.bit.ACQPS = 6; \

\

AdcRegs.ADCSOC6CTL.bit.CHSEL = 2;    /* ChSelect: ADC A2-> Low Side DC Bus Return Cur.*/ \

AdcRegs.ADCSOC6CTL.bit.TRIGSEL = 5; \

AdcRegs.ADCSOC6CTL.bit.ACQPS = 6; \

            \

EDIS; \

\

\

    /* Set up Event Trigger with CNT_zero enable for Time-base of EPWM1 */ \

    EPwm1Regs.ETSEL.bit.SOCAEN = 1;     /* Enable SOCA */ \

    EPwm1Regs.ETSEL.bit.SOCASEL = 1;    /* Enable CNT_zero event for SOCA */ \

    EPwm1Regs.ETPS.bit.SOCAPRD = 1;     /* Generate SOCA on the 1st event */ \

EPwm1Regs.ETCLR.bit.SOCA = 1;       /* Clear SOCA flag */

#endif // __F2806XILEG_VDC_H__

#define ADC_MACRO() \ \ DELAY_US(ADC_usDELAY); \    AdcRegs.ADCCTL1.all=ADC_RESET_FLAG; \ asm(" NOP "); \ asm(" NOP ");    \ \ EALLOW; \ AdcRegs.ADCCTL1.bit.ADCBGPWD = 1; /* Power up band gap */ \ \ DELAY_US(ADC_usDELAY); /* Delay before powering up rest of ADC */ \ \ AdcRegs.ADCCTL1.bit.ADCREFSEL = 0; \    AdcRegs.ADCCTL1.bit.ADCREFPWD = 1; /* Power up reference */ \    AdcRegs.ADCCTL1.bit.ADCPWDN = 1; /* Power up rest of ADC */ \ AdcRegs.ADCCTL1.bit.ADCENABLE = 1; /* Enable ADC */ \ \ asm(" RPT#100 || NOP"); \ \ AdcRegs.ADCCTL1.bit.INTPULSEPOS=1; \ AdcRegs.ADCCTL1.bit.TEMPCONV=0; \ \ DELAY_US(ADC_usDELAY); \ \ /******* CHANNEL SELECT *******/ \ \ \ AdcRegs.ADCSOC0CTL.bit.CHSEL = 1;    /* ChSelect: ADC A1-> Phase U Churrent*/ \ AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 5; /* Set SOC0 start trigger on EPWM1A, due to round-robin SOC0 converts first then SOC1*/ \ AdcRegs.ADCSOC0CTL.bit.ACQPS = 6; /* Set SOC0 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)*/ \ \ AdcRegs.ADCSOC1CTL.bit.CHSEL = 9; /* ChSelect: ADC B1-> Phase V Current*/ \ AdcRegs.ADCSOC1CTL.bit.TRIGSEL  = 5; \ AdcRegs.ADCSOC1CTL.bit.ACQPS = 6; \ \ AdcRegs.ADCSOC2CTL.bit.CHSEL = 10; /* ChSelect: ADC B2-> DC Bus Voltage*/ \ AdcRegs.ADCSOC2CTL.bit.TRIGSEL  = 5; \ AdcRegs.ADCSOC2CTL.bit.ACQPS = 6; \ \ AdcRegs.ADCSOC3CTL.bit.CHSEL = 15; /* ChSelect: ADC B7-> V Phase A */ \ AdcRegs.ADCSOC3CTL.bit.TRIGSEL = 5; \ AdcRegs.ADCSOC3CTL.bit.ACQPS = 6; \ \ AdcRegs.ADCSOC4CTL.bit.CHSEL = 7; /* ChSelect: ADC A7-> V Phase B */ \ AdcRegs.ADCSOC4CTL.bit.TRIGSEL  = 5; \ AdcRegs.ADCSOC4CTL.bit.ACQPS = 6; \ \ AdcRegs.ADCSOC5CTL.bit.CHSEL = 12; /* ChSelect: ADC B4-> V Phase C */ \ AdcRegs.ADCSOC5CTL.bit.TRIGSEL  = 5; \ AdcRegs.ADCSOC5CTL.bit.ACQPS = 6; \ \ AdcRegs.ADCSOC6CTL.bit.CHSEL = 2;    /* ChSelect: ADC A2-> Low Side DC Bus Return Cur.*/ \ AdcRegs.ADCSOC6CTL.bit.TRIGSEL = 5; \ AdcRegs.ADCSOC6CTL.bit.ACQPS = 6; \             \ EDIS; \ \ \    /* Set up Event Trigger with CNT_zero enable for Time-base of EPWM1 */ \    EPwm1Regs.ETSEL.bit.SOCAEN = 1;     /* Enable SOCA */ \    EPwm1Regs.ETSEL.bit.SOCASEL = 1;    /* Enable CNT_zero event for SOCA */ \    EPwm1Regs.ETPS.bit.SOCAPRD = 1;     /* Generate SOCA on the 1st event */ \ EPwm1Regs.ETCLR.bit.SOCA = 1;       /* Clear SOCA flag */

#endif // __F2806XILEG_VDC_H__