新手想请问一下如何使用片外存储器。例如F2407中DS、PS为片选信号,连接了外部ram的片选。A0-A15连接了外部ram的A0-A15地址线,D0-D15也连接了外部ram的D0-D15数据线。(64K的外部存储器)。这时候我应该如何编程使用外部存储器呢,就是编写DS、PS这种片选信号,也没有寄存器可以控制这些信号啊。还有就是如果片选信号接通了是不是在cmd文件中给外部存储区分配了空间就可以使用了呢。因为手册里写的8000-FFFF是外部存储,如果是连接了16位的地址线,也就是64K的外部存储会发生什么...0-7FFF的区域使用的是片内存储还是片外存储。新手没用过,可能有些表述有常识性错误,希望有人帮忙解答一下,急急急,万分感谢!!!