This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377s DMA读取ADC值



现在想通过一个DMA的通道一次读取 A,B,C,D四个ADC模块的值(四个模块各用一个通道),即一次转换结束后四个结果都存在四个模块各自的adcresult0中,通过DMA_ADCAINT2触发DMA转换,然后读取结果,这个方法能否实现?

因为四个ADC模块存放的结果寄存器地址偏移有0x20,

DMACH1AddrConfig(ADCDataBuf,&AdcaResultRegs.ADCRESULT0); AdcaResultRegs.ADCRESULT0的地址为0xB00

DMACH1BurstConfig(3,(0x20-1),511);此配置一次突发传送传递4个字,是否可以理解为是从0xB00,0xB20,0xB40,0xB60中分别读取4个字?

传输512次后目的地址回到初始值,原始地址(0xB00)每次传输都回到原来的地址

以上能否只通过一个DMA通道实现?