This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于28335的ePWM触发中断的疑问????



我想要产生一个三角载波,但是上升和下降的斜率不一样,目前的做法是,利用ePWM1和ePWM2产生两个中断,分别在TBCTR=0和TBCTR=TBPRD的时候进入中断,改变CLKDIV和HSPCLKDIV的值,改变基准时钟分频位,从而改变三角波两边的斜率

EALLOW;
PieVectTable.EPWM1_INT = &OffsetISR;
PieVectTable.EPWM2_INT = &Clk_ISR;
EDIS;

// Enable CNT_zero interrupt using EPWM1 Time-base
EPwm1Regs.ETSEL.bit.INTEN = 1; // Enable EPWM1INT generation 使能产生中断信号EPWMx_INT
EPwm1Regs.ETSEL.bit.INTSEL = 1; // Enable interrupt CNT_zero event 001:TBCTR=0x0000时产生EPWMx_INT
EPwm1Regs.ETPS.bit.INTPRD = 1; // Generate interrupt on the 1st event 中断周期设定,01:每发生一次事件,产生中断信号EPWMx_INT
EPwm1Regs.ETCLR.bit.INT = 1; // Enable more interrupts

// Enable CNT_zero interrupt using EPWM1 Time-base
EPwm2Regs.ETSEL.bit.INTEN = 1; // Enable EPWM1INT generation 使能产生中断信号EPWMx_INT
EPwm2Regs.ETSEL.bit.INTSEL = 2; // Enable interrupt CNT_zero event 001:TBCTR=0xTBPRD时产生EPWMx_INT
EPwm2Regs.ETPS.bit.INTPRD = 1; // Generate interrupt on the 1st event 中断周期设定,01:每发生一次事件,产生中断信号EPWMx_INT
EPwm2Regs.ETCLR.bit.INT = 1; // Enable more interrupts

interrupt void MainISR(void)
{

pwm1.PeriodMax =750;
pwm1.HalfPerMax=pwm1.PeriodMax/2;
pwm1.Deadband = 2.0*SYSTEM_FREQUENCY; // 120 counts -> 2.0 usec for TBCLK = SYSCLK/1

pwm1.Clk = 0;
pwm1.Hspclk =3;
PWM_INIT_MACRO(1,2,3,pwm1);

// Enable more interrupts from this timer
EPwm1Regs.ETCLR.bit.INT = 1;

// Acknowledge interrupt to recieve more interrupts from PIE group 3
PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;

}

interrupt void Clk_ISR(void)
{

pwm1.PeriodMax =750;
pwm1.HalfPerMax=pwm1.PeriodMax/2;
pwm1.Deadband = 2.0*SYSTEM_FREQUENCY; // 120 counts -> 2.0 usec for TBCLK = SYSCLK/1
pwm1.Clk = 0;
pwm1.Hspclk = 7;
PWM_INIT_MACRO(1,2,3,pwm1);

// Enable more interrupts from this timer
EPwm2Regs.ETCLR.bit.INT = 1;

// Acknowledge interrupt to recieve more interrupts from PIE group 3
PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;

}

现在遇到问题是:

1.中断频率与我计算的频率不一致,应该是10KHz的频率,但是实测是9.6KHz,为什么会出现这种情况。

2.每一个ePWM都有各自的时间基准计数器,当ePWM2中断触发(CTL=PRD)的时候,ePWM1的计数器是否也到了CTR=PRD的条件?这样让他们同步?

3.我是在ctr=prd的时候出发了ePWM1_SOC信号,AD开始采样,这与我的ePWM2的中断是否冲突,哪个先执行?