This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于28035的epwm的问题



我用28035实现如下功能: PWM1的计数器为零时触发一路AD采样,为周期时触发另外一路AD采样,同时PWM1和PWM2的计数器是同步的。具体设置见下面。

问题是:PWM1的计数器为零时触发AD采样和PWM1和PWM2的计数器同步两个同时存在时,则pwm输出完全乱掉了,不只是pwm1和pwm2,连pwm3和pwm6都乱掉了,如果注释掉红字的一行或者绿色的三行都能正常运行。就是说pwm1过零时同时触发ad和pwm同步信号就有问题,而单独执行一个就ok,我在手册里没有看到说这两个不能同时设置。

请问上述问题是我设置不对还是别的问题?有没有好的解决办法?

EPwm3Regs.TBPRD = 3124;

 EPwm3Regs.TBPHS.half.TBPHS = 0x0000;

 EPwm3Regs.TBCTR = 0x0000;

 EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;

 EPwm3Regs.TBCTL.bit.PHSEN = TB_DISABLE;

 EPwm3Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;

 EPwm3Regs.TBCTL.bit.CLKDIV = TB_DIV1;

 EPwm3Regs.CMPA.half.CMPA = 1500;

 EPwm3Regs.AQCTLB.all = 0x0018;

 

 EPwm6Regs.TBPRD = 3124;

 EPwm6Regs.TBPHS.half.TBPHS = 0x0000;

 EPwm6Regs.TBCTR = 0x0000;

 EPwm6Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;

 EPwm6Regs.TBCTL.bit.PHSEN = TB_DISABLE;

 EPwm6Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;

 EPwm6Regs.TBCTL.bit.CLKDIV = TB_DIV1; 

 EPwm6Regs.CMPA.half.CMPA = 0;

 EPwm6Regs.AQCTLB.all = 0x0018;

 

 

 EPwm1Regs.TBPRD = 1500;

 EPwm1Regs.TBPHS.half.TBPHS = 0x0000;

 EPwm1Regs.TBCTR = 0x0000;

 EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;

 EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE;

 EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;

 EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW;

 EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;

EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO;

 EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD;

 EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_PRD;

 EPwm1Regs.CMPA.half.CMPA = 0;

 EPwm1Regs.CMPB = 0;

 EPwm1Regs.AQCTLA.all = 0x0090;

 EPwm1Regs.AQCTLB.all = 0x0900;

 

 EPwm1Regs.ETSEL.bit.SOCAEN  = 1;

 EPwm1Regs.ETSEL.bit.SOCASEL = 1;

 EPwm1Regs.ETSEL.bit.SOCBEN  = 1;

 EPwm1Regs.ETSEL.bit.SOCBSEL = 2;

 EPwm1Regs.ETPS.bit.SOCAPRD  = 1;

 EPwm1Regs.ETPS.bit.SOCBPRD  = 1;

 

 EPwm2Regs.TBPRD = 1500;

 EPwm2Regs.TBPHS.half.TBPHS = 0x0000;

 EPwm2Regs.TBCTR = 0x0000;

 EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;

 EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE;

 EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;

 EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;

 EPwm2Regs.TBCTL.bit.PRDLD = TB_SHADOW;

// EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE;

 EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD;

 EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_PRD;

 EPwm2Regs.CMPA.half.CMPA = 0;

 EPwm2Regs.CMPB = 0;

 EPwm2Regs.AQCTLA.all = 0x0090;

 EPwm2Regs.AQCTLB.all = 0x0900;

  • 应该是可以设置的,但也没看出来你的代码有什么问题,不知道你说的PWM输出乱了是个具体的什么情况?

    另外,是否有在以上的ePWM初始化之前先关闭同步时钟信号(EALLOW;SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0; EDIS;),初始化完之后再打开(EALLOW;SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1; EDIS;)?

    如果可以,建议将程序简化以排除其它因素的影响(猜测是某些顺序导致?),或者将整个工程共享出来测试一下。