This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于28027F 使用硬件I2C读写EEPROM的问题

Other Parts Discussed in Thread: MOTORWARE

代码是从controlsuit例程直接移植到motorware例程中的,配置完全一样,但是例程可以正常读写,移进motorware之后,测试引脚都没有信号,这是为什么呢?使用的是controlsuit例程中的 i2c.c 和 i2c.h。

在motor ware lab4中配置I2C如下:

在hal_init函数中:

obj->i2cHandle = I2C_init((void *)I2CA_BASE_ADDR,sizeof(I2C_Obj));

在hal_setup函数中: // I2C void HAL_setupI2C(HAL_Handle handle) { HAL_Obj *obj = (HAL_Obj *)handle; // Slave address - EEPROM control code I2C_setMasterSlaveAddr(obj->i2cHandle, 0x0050); // I2CCLK = SYSCLK/(I2CPSC+1) // Prescaler - need 7-12 Mhz on module clk // 模块时钟 10MHz;主机时钟 400K,高电平1.5us,低电平1us I2C_setupClock(obj->i2cHandle, 6, 5, 10); // Enable SCD & ARDY interrupts I2C_enableInt(obj->i2cHandle, I2C_IntEn_Stop); I2C_enableInt(obj->i2cHandle, I2C_IntEn_Reg_Rdy); // Take I2C out of reset, enable I2C // Stop I2C when suspended I2C_enable(obj->i2cHandle); // Enable FIFO mode and TXFIFO I2C_enableFifo(obj->i2cHandle); I2C_resetTxFifo(obj->i2cHandle); // Enable RXFIFO, clear RXFFINT I2C_resetRxFifo(obj->i2cHandle); I2C_clearRxFifoInt(obj->i2cHandle); // Enable I2C interrupt 1 in the PIE: Group 8 interrupt 1 PIE_enableInt(obj->pieHandle, PIE_GroupNumber_8, PIE_InterruptSource_I2CA1); // Enable CPU INT8 which is connected to PIE group 8 CPU_enableInt(obj->cpuHandle, CPU_IntNumber_8); return; }
I2C IO设置: // I2C端口配置 GPIO_setPullUp(obj->gpioHandle, GPIO_Number_32, GPIO_PullUp_Enable); GPIO_setPullUp(obj->gpioHandle, GPIO_Number_33, GPIO_PullUp_Enable); GPIO_setQualification(obj->gpioHandle, GPIO_Number_32, GPIO_Qual_ASync); GPIO_setQualification(obj->gpioHandle, GPIO_Number_33, GPIO_Qual_ASync); GPIO_setMode(obj->gpioHandle, GPIO_Number_32, GPIO_32_Mode_SDAA); GPIO_setMode(obj->gpioHandle, GPIO_Number_33, GPIO_33_Mode_SCLA);
开启I2C外设时钟: CLK_enableI2cClock(obj->clkHandle);
配置中断向量表: pie->I2CINT1A = &i2ca1_isr;
中断函数: interrupt void i2ca1_isr(void) { uint16_t IntSource, i; // Read interrupt source IntSource = I2C_getIntSource(halHandle->i2cHandle); // Interrupt source = stop condition detected if(IntSource == I2C_IntSrc_Stop) // 检测到STP=1,中断开始(SCD中断) { // If completed message was writing data, reset msg to inactive state if(CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_WRITE_BUSY) // 发送完成,设置为未启动状态,可以进行下一次写数据 CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_INACTIVE; else { // If a message receives a NACK during the address setup portion of the // EEPROM read, the code further below included in the register access ready // interrupt source code will generate a stop condition. After the stop // condition is received (here), set the message status to try again. // User may want to limit the number of retries before generating an error. if(CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP_BUSY) CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_SEND_NOSTOP; // If completed message was reading EEPROM data, reset msg to inactive state // and read data from FIFO. else if(CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_READ_BUSY) // 读数据完成。可读取I2C FIFO寄存器数据 { // 设置为未启动状态,允许下一次读写 EEPROM CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_INACTIVE; for(i=0; i < I2C_NUMBYTES; i++) CurrentMsgPtr->MsgBuffer[i] = I2C_getData(halHandle->i2cHandle); // Check received data for(i=0; i < I2C_NUMBYTES; i++) { if(I2cMsgRead.MsgBuffer[i] == I2cMsgWrite.MsgBuffer[i]) PassCount++; else FailCount++; } if(PassCount == I2C_NUMBYTES) { __asm(" ESTOP0"); for(;;); } else { __asm(" ESTOP0"); for(;;); } } } } // end of stop condition detected // Interrupt source = Register Access Ready // This interrupt is used to determine when the EEPROM address setup portion of the // read data communication is complete. Since no stop bit is commanded, this flag // tells us when the message has been sent instead of the SCD flag. If a NACK is // received, clear the NACK bit and command a stop. Otherwise, move on to the read // data portion of the communication. // ARDY中断:①收到 NACK 回复,产生停止位使得长生 SCD 中断; // ②在非重复模式中,当没有检测到停止位 STP=0,内部计数器向下计数到 0,ARDY 置位(产生 ARDY 中断); else if(IntSource == I2C_IntSrc_Reg_Rdy) { if(I2C_getStatus(halHandle->i2cHandle) == I2C_Status_NACK) // EEPROM处理数据忙回复 NACK { I2C_MasterControl(halHandle->i2cHandle, I2C_Control_Stop, I2C_BitCount_8_Bits, 0); // 产生一个 STOP 停止位,引发一次 SCD 中断 I2C_clearSTR_NACK_flag(halHandle->i2cHandle); // 清除 NACK位 } // 发送完成数据,没有停止位,收到回复 ACK,内部计数为零,产生 ARDY 中断 else if(CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP_BUSY) CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_RESTART; // 更新为重发 START 位状态,为接收数据准备 } // end of register access ready else { // Generate some error due to invalid interrupt source __asm(" ESTOP0"); } // Enable future I2C (PIE Group 8) interrupts PIE_clearInt(halHandle->pieHandle, PIE_GroupNumber_8); return; }
I2C 使用相关定义: #define I2C_EEPROM_Block0_ADDRESS 0x50 #define I2C_EEPROM_HIGH_ADDR 0x00 // 数据地址高位,变化范围 0x00 ~ 0x03 #define I2C_EEPROM_LOW_ADDR 0x00 // 数据地址低位,变化范围 0x00 ~ 0xFF // Error Messages #define I2C_ERROR 0xFFFF #define I2C_ARB_LOST_ERROR 0x0001 #define I2C_NACK_ERROR 0x0002 #define I2C_BUS_BUSY_ERROR 0x1000 #define I2C_STP_NOT_READY_ERROR 0x5555 #define I2C_NO_FLAGS 0xAAAA #define I2C_SUCCESS 0x0000 // I2CMSG structure defines #define I2C_MAX_BUFFER_SIZE 4 // 定义数据存取长度 #define I2C_NUMBYTES 2 // 传输字节数 // I2C Message Commands for I2CMSG struct #define I2C_MSGSTAT_INACTIVE 0x0000 // 未激活:发送成功或接收成功后设置,允许下一次发送或接收数据。 #define I2C_MSGSTAT_SEND_WITHSTOP 0x0010 // 带停止位发送:用于数据写入,停止位表示写入完成。 #define I2C_MSGSTAT_WRITE_BUSY 0x0011 // 写数据忙:数据移入缓冲器后使能IIC发送,并设置为此状态,表示数据正在传输, // 可通过查询SCD位判断是否传送完毕。 #define I2C_MSGSTAT_SEND_NOSTOP 0x0020 // 无停止位发送:用于读取数据,发送设备地址后还需发送数据地址,因此不能产生停止位, // 发送设备地址后设为此状态,表示可以发送数据地址。 #define I2C_MSGSTAT_SEND_NOSTOP_BUSY 0x0021 // 发送无停止位忙:用于读取数据,表示地址已经在传送中,可通过ARDY标志判断是否传送成功。 #define I2C_MSGSTAT_RESTART 0x0022 // 重发开始为:用于读取数据,表示地址传送成功,可以重发设备地址并接收EEPROM的数据 // 到缓冲区,接收完成设定的数据个数发送停止位停止数据传输。 // 注:写完数据并不能马上读取,EEPROM需要一定的时间存取数据,2ms左右; // 因此发送设备地址和数据地址需要执行多次,才能得到 ACK,然后读取数据。 #define I2C_MSGSTAT_READ_BUSY 0x0023 // 读取数据忙:用于读取数据,在第二次发送START+设备地址后设为此状态, // 表示IIC已经开始接收数据,可通过ARDY判断是否接收成功。 //------------ // Structures //------------ // I2C Message Structure typedef struct _I2CMSG_t_ { uint16_t MsgStatus; // Word stating what state msg is in: // I2C_MSGCMD_INACTIVE = do not send msg // I2C_MSGCMD_BUSY = msg start has been sent, // awaiting stop // I2C_MSGCMD_SEND_WITHSTOP = command to send // master trans msg complete with a stop bit // I2C_MSGCMD_SEND_NOSTOP = command to send // master trans msg without the stop bit // I2C_MSGCMD_RESTART = command to send a restart // as a master receiver with a stop bit uint16_t SlaveAddress; // I2C address of slave msg is intended for uint16_t MemoryHighAddr; // EEPROM address of data associated with msg (high byte) uint16_t MemoryLowAddr; // EEPROM address of data associated with msg (low byte) uint16_t MsgBuffer[I2C_MAX_BUFFER_SIZE]; // Array holding msg data - max that // MAX_BUFFER_SIZE can be is 4 due to the FIFO's }I2CMSG_t;
I2C读写文件: /* * I2C_EE.c * I2c EEPROM(AT24C08D) 应用函数 */ #include "I2C_EE.h" #include "i2c.h" uint16_t PassCount=0; uint16_t FailCount=0; I2CMSG_t I2cMsgWrite={I2C_MSGSTAT_SEND_WITHSTOP, I2C_EEPROM_Block0_ADDRESS, I2C_EEPROM_HIGH_ADDR, I2C_EEPROM_LOW_ADDR, 0x12, // Msg Byte 01 0x34}; // Msg Byte 02 I2CMSG_t I2cMsgRead={I2C_MSGSTAT_SEND_NOSTOP, I2C_EEPROM_Block0_ADDRESS, I2C_EEPROM_HIGH_ADDR, I2C_EEPROM_LOW_ADDR, 0x00, 0x00}; // Used in interrupts I2CMSG_t *CurrentMsgPtr=&I2cMsgWrite; I2C_Handle i2cHandle; static inline uint16_t I2CA_WriteData(I2CMSG_t *msg, uint16_t NumByteToWrite) { uint16_t i; // Wait until the STP bit is cleared from any previous master communication. // Clearing of this bit by the module is delayed until after the SCD bit is // set. If this bit is not checked prior to initiating a new message, the // I2C could get confused. if(I2C_checkMasterStop(i2cHandle) == 1) return I2C_STP_NOT_READY_ERROR; // Setup slave address I2C_setMasterSlaveAddr(i2cHandle, msg->SlaveAddress); // Check if bus busy if(I2C_isMasterBusy(i2cHandle) == 1) return I2C_BUS_BUSY_ERROR; // Setup number of bytes to send // Send start as master transmitter I2C_enable(i2cHandle); I2C_enable_FREE(i2cHandle); I2C_MasterControl(i2cHandle, I2C_Control_Single_TX, I2C_BitCount_8_Bits, (NumByteToWrite + 2)); // Setup data_adress to send I2C_putData(i2cHandle, msg->MemoryHighAddr); I2C_putData(i2cHandle, msg->MemoryLowAddr); for(i=0; i<NumByteToWrite; i++) { I2C_putData(i2cHandle, *(msg->MsgBuffer+i)); // 若FIFO满,则等待(避免FIFO溢出覆盖先前数据) while(I2C_getTxFifoStatus(i2cHandle) == I2C_FifoStatus_4_Words); } msg->MemoryLowAddr += i;//just for test return I2C_SUCCESS; } static inline uint16_t I2CA_ReadData(I2CMSG_t *msg, uint16_t NumByteToRead) { // Wait until the STP bit is cleared from any previous master communication. // Clearing of this bit by the module is delayed until after the SCD bit is // set. If this bit is not checked prior to initiating a new message, the // I2C could get confused. if(I2C_checkMasterStop(i2cHandle) == 1) return I2C_STP_NOT_READY_ERROR; // Setup slave address I2C_setMasterSlaveAddr(i2cHandle, msg->SlaveAddress); if(msg->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP) // 产生第一个START位后发送设备地址和数据地址 { // Check if bus busy if(I2C_isMasterBusy(i2cHandle) == 1) return I2C_BUS_BUSY_ERROR; I2C_MasterControl(i2cHandle, I2C_Control_Burst_TX_Start, I2C_BitCount_8_Bits, NumByteToRead); I2C_enable(i2cHandle); // Send data to setup EEPROM address I2C_putData(i2cHandle, msg->MemoryHighAddr); I2C_putData(i2cHandle, msg->MemoryLowAddr); } else if(msg->MsgStatus == I2C_MSGSTAT_RESTART) // 产生第二个START位后发送设备地址并开始接收数据 { // Setup how many bytes to expect // Send restart as master receiver I2C_MasterControl(i2cHandle, I2C_Control_Single_RX, I2C_BitCount_8_Bits, NumByteToRead); I2C_enable(i2cHandle); } return I2C_SUCCESS; } // Write data to EEPROM section void I2C_EE_Write(I2CMSG_t *msg, uint16_t NumByteToWrite) { uint16_t Error; // Check the outgoing message to see if it should be sent. // In this example it is initialized to send with a stop bit. if(msg->MsgStatus == I2C_MSGSTAT_SEND_WITHSTOP) { Error = I2CA_WriteData(msg, NumByteToWrite); // If communication is correctly initiated, set msg status to busy // and update CurrentMsgPtr for the interrupt service routine. // Otherwise, do nothing and try again next loop. Once message is // initiated, the I2C interrupts will handle the rest. Search for // ICINTR1A_ISR in the i2c_eeprom_isr.c file. if(Error == I2C_SUCCESS) { CurrentMsgPtr = msg; msg->MsgStatus = I2C_MSGSTAT_WRITE_BUSY; } } // end of write section } // Read data from EEPROM section void I2C_EE_Read(I2CMSG_t *msg, uint16_t NumByteToRead) { // 读数据包括两次发送 START 位,第一次发送地址 // Check outgoing message status. Bypass read section if status is not inactive. if(I2cMsgWrite.MsgStatus == I2C_MSGSTAT_INACTIVE) { // Check incoming message status. if(msg->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP) { // EEPROM address setup portion while(I2CA_ReadData(msg, 2) != I2C_SUCCESS) { // Maybe setup an attempt counter to break an infinite while // loop. The EEPROM will send back a NACK while it is performing // a write operation. Even though the write communique is // complete at this point, the EEPROM could still be busy // programming the data. Therefore, multiple attempts are necessary. // 需要一定是时间完成数据的烧写,1.8ms左右;需要多次尝试,直到返回 ACK 确认。 } // Update current message pointer and message status CurrentMsgPtr = msg; msg->MsgStatus = I2C_MSGSTAT_SEND_NOSTOP_BUSY; } // Once message has progressed past setting up the internal address // of the EEPROM, send a restart to read the data bytes from the // EEPROM. Complete the communique with a stop bit. MsgStatus is // updated in the interrupt service routine. else if(msg->MsgStatus == I2C_MSGSTAT_RESTART) { // Read data portion while(I2CA_ReadData(msg, NumByteToRead) != I2C_SUCCESS) { // Maybe setup an attempt counter to break an infinite while loop. } // Update current message pointer and message status CurrentMsgPtr = msg; msg->MsgStatus = I2C_MSGSTAT_READ_BUSY; } } // end of read section }