This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28335的485通信问题

大家好,最近在调试28335的485通信,通过GPIO26控制ADM2582E芯片进行收发数据,DPIO26为高电平时发数,低电平时收数,采用Scib通道。在TI例程基础上修改如下:

#include "DSP28x_Project.h" // Device Headerfile and Examples Include File


void Scib_echoback_init(void);
void Scib_fifo_init(void);
void Scib_xmit(int a);
void Scib_msg(char *msg);
void delay(Uint16 count);
void Gpio_select(void);

Uint16 LoopCount;
Uint16 ErrorCount;

void main(void)
{
Uint16 ReceivedChar;
char *msg;

InitSysCtrl();

InitScibGpio();

DINT;

InitPieCtrl();


IER = 0x0000;
IFR = 0x0000;


InitPieVectTable();

LoopCount = 0;
ErrorCount = 0;

EALLOW;

GpioCtrlRegs.GPAPUD.bit.GPIO26= 0;
GpioCtrlRegs.GPAMUX2.bit.GPIO26= 0; 
GpioCtrlRegs.GPADIR.bit.GPIO26= 1;
GpioDataRegs.GPASET.bit.GPIO26= 1; 

EDIS;

Scib_fifo_init(); // Initialize the SCI FIFO
Scib_echoback_init(); // Initialize SCI for echoback


GpioDataRegs.GPASET.bit.GPIO26= 1;
delay(200);


delay(200);
msg = "\r\n\n\nHello World!\0";
Scib_msg(msg); 

msg = "\r\nYou will enter a character, and the DSP will echo it back! \n\0";
Scib_msg(msg); //TX

for(;;)
{
GpioDataRegs.GPASET.bit.GPIO26 = 1;
delay(200);

msg = "\r\nEnter a character: \0";
Scib_msg(msg);

GpioDataRegs.GPACLEAR.bit.GPIO26 = 1;
while(ScibRegs.SCIFFRX.bit.RXFFST !=1) { } // wait for XRDY =1 for empty state

ReceivedChar = ScibRegs.SCIRXBUF.all;
GpioDataRegs.GPASET.bit.GPIO26 = 1;

msg = " You sent: \0";
Scib_msg(msg);
delay(200);
Scib_xmit(ReceivedChar); //RX
GpioDataRegs.GPASET.bit.GPIO26 = 1;
delay(200);
LoopCount++;
}
}

// Test 1,Scib DLB, 8-bit word, baud rate 0x000F, default, 1 STOP bit, no parity
void Scib_echoback_init()
{
// Note: Clocks were turned on to the Scib peripheral
// in the InitSysCtrl() function

ScibRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
ScibRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
// ScibRegs.SCICTL2.all =0x0003;
ScibRegs.SCICTL2.bit.TXINTENA =1;
ScibRegs.SCICTL2.bit.RXBKINTENA =1;
// #if (CPU_FRQ_150MHZ)
ScibRegs.SCIHBAUD =0x0001; // 9600 baud @LSPCLK = 37.5MHz.
ScibRegs.SCILBAUD =0x00E7;
// #endif

ScibRegs.SCIFFTX.all=0x801f;//0xe040;
ScibRegs.SCIFFRX.all=0x001f;
ScibRegs.SCIFFCT.all=0x00;

ScibRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
}

// Transmit a character from the SCI
void Scib_xmit(int a)
{
while (ScibRegs.SCIFFTX.bit.TXFFST != 0) {}
ScibRegs.SCITXBUF=a;
}

void Scib_msg(char * msg)
{
int i;
i = 0;
while(msg[i] != '\0')
{
Scib_xmit(msg[i]);
i++;
}
}

// Initialize the SCI FIFO
void Scib_fifo_init()
{
ScibRegs.SCIFFTX.all=0xE040;
ScibRegs.SCIFFRX.all=0x204f;
ScibRegs.SCIFFCT.all=0x0;
}

void delay(Uint16 count) /*count=1 about 0.1us */
{
while(count>0)
{
count--;
asm(" NOP");
asm(" NOP");
asm(" NOP");
asm(" NOP");
asm(" NOP");
asm(" NOP");
}
}

但是实现不了485通信功能,希望大家能帮忙找找原因,不胜感激。

  • 先测测loopback能不能通,看一下链路上信号
  • 您好!按照您的建议采用了loopback进行测试,其中ReceivedChar是依次递增的,但仍然接收不到数据,代码如下:
    #include "DSP28x_Project.h" // Device Headerfile and Examples Include File

    // Prototype statements for functions found within this file.
    void Scib_loopback_init(void);
    void Scib_fifo_init(void);
    void Scib_xmit(int a);
    void error();
    __interrupt void Scib_rx_isr(void);
    __interrupt void Scib_tx_isr(void);
    void delay(Uint16 count);
    // Global counts used in this example
    Uint16 LoopCount;
    Uint16 ErrorCount;

    void main(void)
    {
    Uint16 SendChar;
    Uint16 ReceivedChar;


    InitSysCtrl();


    InitSciGpio();

    DINT;
    IER = 0x0000;
    IFR = 0x0000;

    InitPieVectTable();

    EnableInterrupts();

    LoopCount = 0;
    ErrorCount = 0;

    Scib_fifo_init(); // Initialize the SCI FIFO
    Scib_loopback_init(); // Initialize SCI for digital loop back

    SendChar = 0;
    EALLOW;
    GpioCtrlRegs.GPAPUD.bit.GPIO26= 0;
    GpioCtrlRegs.GPAMUX2.bit.GPIO26= 0;
    GpioCtrlRegs.GPADIR.bit.GPIO26= 1; // output
    GpioDataRegs.GPASET.bit.GPIO26= 1; // Load output latch
    EDIS;
    for(;;)
    {
    Scib_xmit(SendChar);
    delay(100);
    GpioDataRegs.GPACLEAR.bit.GPIO26= 1;
    delay(100);
    while(ScibRegs.SCIFFRX.bit.RXFFST !=1) { } // wait for RRDY/RXFFST =1 for 1 data available in FIFO

    ReceivedChar = ScibRegs.SCIRXBUF.all;
    GpioDataRegs.GPASET.bit.GPIO26= 1;
    delay(100);
    if(ReceivedChar != SendChar) error();
    SendChar++;
    SendChar &= 0x00FF;
    LoopCount++;
    }
    }

    void error()
    {
    ErrorCount++;
    // __asm(" ESTOP0"); // Uncomment to stop the test here
    // for (;;);
    }

    // Test 1,Scib DLB, 8-bit word, baud rate 0x000F, default, 1 STOP bit, no parity
    void Scib_loopback_init()
    {
    // Note: Clocks were turned on to the Scib peripheral
    // in the InitSysCtrl() function

    ScibRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback
    // No parity,8 char bits,
    // async mode, idle-line protocol
    ScibRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK,
    // Disable RX ERR, SLEEP, TXWAKE
    ScibRegs.SCICTL2.all =0x0003;
    ScibRegs.SCICTL2.bit.TXINTENA =1;
    ScibRegs.SCICTL2.bit.RXBKINTENA =1;
    ScibRegs.SCIHBAUD =0x0001;
    ScibRegs.SCILBAUD =0x00E7;
    ScibRegs.SCICCR.bit.LOOPBKENA =1; // Enable loop back
    ScibRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
    }

    // Transmit a character from the SCI'
    void Scib_xmit(int a)
    {
    ScibRegs.SCITXBUF=a;
    }

    // Initialize the SCI FIFO
    void Scib_fifo_init()
    {
    ScibRegs.SCIFFTX.all=0xe040;
    ScibRegs.SCIFFRX.all=0x204f;
    ScibRegs.SCIFFCT.all=0x0;
    }

    void delay(Uint16 count) /*count=1 about 0.1us */
    {
    while(count>0)
    {
    count--;
    asm(" NOP");
    asm(" NOP");
    asm(" NOP");
    asm(" NOP");
    asm(" NOP");
    asm(" NOP");
    }
    }
    是不是SCIB和SCIA使用有区别呢?谢谢!
  • 对28335来讲 其实就是SCI接口啊 你先将485端收发短接 看看自发自收有没有问题
    如果还有问题 你看看总线上的数量 是否全双工等