This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于F28M35中的EPI总线接口的EPI0S33和EPI0S34信号的管脚



最近需要使用F28M35的EPI总线扩展四个外围设备,使用HB8的复用模式,外接CS0-CS3时,发现CS2和CS3找不到对应的GPIO管脚。手册(Technical Reference Manual)中是EPI0S33和EPI0S34信号。在GPIO管脚复用模块中,却没有这两个信号可在GPIO中复用。

在数据手册中,4.2的Terminal Functions中,EPI0S33和EPI0S34等全部的EPI0S32至EPI0S41的信号却又分配了对应的管脚,比如S33是分配在GPIO35上的。但是就是不知道如何配置哪个寄存器可以将该信号连接外部管脚。

所以,就觉得有两个疑惑:

1.究竟CS2(EPI0S34)和CS3(EPI0S33)的信号有没有通过管脚互联模块(MUX)连接到外部的GPIO管脚。换言之,我能不能外扩4个外部接口电路(同一型号)。

2.如果不行,有什么其他好的建议,我怎么实现这四个外部电路接口的扩展。

3.如果可以,我应该怎么配置外部管脚互联模块的寄存器。还望TI的工程师帮忙解答一下。如果工作较忙,还请转发其他同事,帮忙解答一下。万分感谢。