This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

motorware例程问题,LAB_13e电机不转



我用的直流伺服电机,采用的drv8301kit_revD+28069miso开发板,用LAB_06a例程电机可以转,但我是要用这个电机进行精确的位置控制,所以电机上配有旋转变压器,采用LAB_13e的例程,通电运行程序,电机不转,每隔2秒左右先逆时针旋转一个角度又马上顺时针转回原来的位置,不知道是什么原因?我旋转电机,观察enc.enc_elec_angle的值变化是正确的,说明解码器工作正常。无感和有感电机的参数现同,我在LAB_13e例程里,把Flag_enableUserParams设为false,看到电机在识别过程中还能运转,但识别结束后电机依然不能运转。

请专家指导我下面要怎么做才能找到问题原因?

谢谢!

  • 请到TI官网搜索InstaSPIN Projects and Labs User’s Guide并参考其说明。
  • 谢谢Seven Han的回复,你说的是instaspin_labs.pdf这个文档吗?

    我在选择Projects 时,就是参考了这个文档才选择的LAB_13e,实际上我从12a,12b,13a,13b都试过了,都是按照instaspin_labs.pdf的方法测试的,但电机始终不转,我观察了,只要给定电机转速IqRef_A就达到了最大值(SpinTAC.VelCtlOutputMax_A),电机好像卡死,把转速设的很低也是这样,我很郁闷,请帮忙分析是什么原因造成的呢?

    我也怀疑过电机UVW线接错,我把这3根线的6种接法都试过了,现象是一样的。

    请Seven Han和有经验的工程师帮忙指导下,谢谢!

  • 现在可以肯定是因为IqRef_A电流过大造成,但实际电流不大,比如IqRef_A电流达到了5.0A,但实测电源电流只有0.4A,是AD采集的不准吗?

  • 我用的直流伺服电机,采用的drv8301kit_revD+28069miso开发板,用LAB_06a例程电机可以转,但我是要用这个电机进行精确的位置控制,所以电机上配有旋转变压器,采用LAB_13e的例程,通电运行程序,电机不转,每隔2秒左右先逆时针旋转一个角度又马上顺时针转回原来的位置,不知道是什么原因?我旋转电机,观察enc.enc_elec_angle的值变化是正确的,说明解码器工作正常。无感和有感电机的参数现同,我在LAB_13e例程里,把Flag_enableUserParams设为false,看到电机在识别过程中还能运转,但识别结束后电机依然不能运转

    ERIC:
    我觉得问题应该是出在你的角度反馈这里。建议你先用无传感Lab05B先跑一下,然后看看FAST识别出来的角度和你用旋转变压器测出来的电角度之间有什么差别。
    调整好之后,先跑一下LAB12B 用带传感器的方式先跑一下速度环,然后再转为MOTION的方式。