This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS6.0编译出现 creating output section ".sysmem" without a SECTIONS 警告

CCS6.0编译出现 creating output section ".sysmem" without a SECTIONS警告

  • .sysmem在SECTIONS没有分配内存空间。
    Warning: creating output section "xxx" without a SECTIONS specification

    This warning means that the linker is creating and allocating output section "xxx" in memory using some default algorithm because it isn't explicitly allocated in the linker command file. While this may be ok, it is generally not advisable. It is best to explicitly allocate the section to the appropriate memory region by adding the section to the SECTIONS directive in the linker command file.