大家在做伺服控制系统的时候是如何考虑用多少位的AD的呢
除了28377 28379之外的C2000控制器一般配12位的片内AD
但是也有不少系统采用片外AD,比如片外16位AD,FPGA控制AD采样,FPGA把AD采集结果传输给C2000控制器
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家在做伺服控制系统的时候是如何考虑用多少位的AD的呢
除了28377 28379之外的C2000控制器一般配12位的片内AD
但是也有不少系统采用片外AD,比如片外16位AD,FPGA控制AD采样,FPGA把AD采集结果传输给C2000控制器
您好 感谢帮助
我现在调试的系统没有用28335片内AD,而是采用FPGA控制外部16bit高速AD采样
我的位置控制要达到小于等于10urad(0.000573)的精度
我想知道16位的AD是否合理
传感器用LEM的 输出2.5V加减0.625V的信号,通过运放将此信号调整到0到5V供AD采集
被控对象是两台24对极永磁同步电机
您好 感谢帮助
您指的有效位数是怎么确定的呢 是根据经验或者考虑的采样噪声或误差得出的吗