This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于28377s的USB接口设计问题



各位专家,请麻烦指导一下关于28377S的USB接口设计,28377s的USB接口是不是既可以作为HOST也可以作为DEVICE端,

如果作为DEVICE端是不是我必须要对主端供给的VBUS电压进行检测,如果作为HOST端,是不是也要对输出的VBUS进行限流

控制?    如果有参考设计请麻烦提供一下? 谢谢