This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35H52C1开发板用ARM核能实时监控吗?



如题。

另外,我要用ARM那边跑程序,需不需要练J8的跳帽?

外接开发板XDS100v2是用于DSP的吗?能不能跑USB的程序?

谢谢!

  • 楼主,请将问题描述详细一些,用ARM核做什么样的实时监控呢?

    J8是值哪里的跳线?USB Docking 上吗?

    XDS100V2仿真器,可以放F28M35H52C1的M3核和C28核。当然也可以仿真M3核的USB程序。

  • 回楼上的话,我还是悲催的在跑device_keyboard例程,运行程序的时候不能用实时模式,工具栏的那2个模式转换的像闹钟一样的按钮是灰色的。

    J8是docking station上的。

    另外,我还想问一下,跑这个例程的时候还需不需要改一下程序?load project后直接运行就行了吗?我怎么进行host 与 device之间的互动呢?

    谢谢!

  • “工具栏的那2个模式转换的像闹钟一样的按钮”只对c2000核有效,对ARM核是无效的。