我手里有一个F28335的板子,DSP通过SPI端口连接了型号为M25P128的FLASH,进行读写测试时遇到问题。DSP向FLASH中写入256字节的测试数据,然后由DSP从FLASH中将这些数据读出,与原始数据进行对比检查是否一致。现在的现象是:将芯片擦除后,DSP从FLASH中读出的数据是0xFF(正确),但只要向FLASH中写入数据,无论这些数据内容是什么,并且无论对哪个PAGE进行操作,在DSP从FLASH中读出的数据中,第1个字节总是0x04,第2~256字节的值与写入的数据一致。用示波器观察过SIMO和SOMI,能够确认DSP写出的数据正确,而FLASH送出的数据中第1个字节的确是0x04。已经被这个问题纠缠很久了,希望大家给予帮助。