This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

大功率PMSM相电流毛刺太多



如题,用28335做了一套60kW永磁同步电机(表贴式)控制器,采用id=0控制模式,发现相电流波形毛刺太大,下图1是送入AD引脚处的电流(交流耦合测试),图2是套在电机绕组上的传感器测出来的波形。

由于功率较大,相电流采集方式是在绕组A/B上外挂LEM电流型传感器,硬件电路上有RC滤波,软件上未用滤波,即在进行CLARK变化时用的AD值就是官网的例程语句:

clarke1.As=((AdcMirror.ADCRESULT1)*0.00024414-offsetA)*2*0.909; // Phase A curr.

请问各位专家,这个电流毛刺该如何削弱一些,在不影响实时性的情况下,AD软件滤波有什么好的方式吗