ccs5.2在断开仿真器连接时,经常死机,是什么原因
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
楼主你好!
我使用CCS V 5.2.0.00057 和CCS V 5.2.0.00069都没有碰到你说的这个问题,也许跟你使用的仿真器有关,请问你使用什么仿真器?CCS V5.2具体版本是?
你好,我使用的是ccs5.2.1.00018 和闻亭的XDS560V2仿真器,发现连接上如果不运行时断开没有问题,如果运行以后停止在断开,就经常发生ccs卡死的状况
楼主可以尝试以下,我目前使用XDS100仿真器和CCS V5.2.0.00069没有这个问题,非常稳定。
1.换其它仿真器试一下,很有可能是仿真器的问题。
2.重新安装ccs5.2.1.00018试一下。
3.换其它版本CCSV5.2试一下。
4.楼主电脑配置是否足够,运行CCS后,电脑是否反映慢?