This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28027 digital_power 库中f2802x_v3.5版本需要配合device support 文件夹中的哪个一个版本的外设库?



1,开发环境CCS8.1 使用digtal_power库中f2802x_v3.2版本配合device support文件夹中V129文件使用可以正确产出PWM波形,pwm寄存器值也是正确的。

2,开发环境CCS8.1 使用digtal_power库中f2802x_v3.5版本配合device support文件夹中V230文件使用不能正确的产生PWM波形,此时pwm寄存器中CMPA,CMPB一直是0,程序能正确进入ISR.asm中断并执行了;”Call” the Run macro 例如PWMDRV_ComplPairDB 1

请求帮助如下:

1,如果使用f2802x_v3.5的库需要选择device support文件夹中哪个版本?

2,是否有推荐的电源库函数版本号?和外设库函数版本号?谢谢!