This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335定时器中断进不去

Other Parts Discussed in Thread: CONTROLSUITE

#include "DSP2833x_Device.h" // Headerfile Include File
#include "DSP2833x_Examples.h" // Examples Include File
interrupt void ISRTimer0(void);
int AA=0;

int main(void)
{
InitSysCtrl();
DINT;
IER=0x0000;
IFR=0X0000;
InitPieVectTable();
InitPieCtrl();
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.TINT0 = &ISRTimer0;
EDIS;
InitCpuTimers();
ConfigCpuTimer(&CpuTimer0,150,500000);
StartCpuTimer0();
PieCtrlRegs.PIEIER1.bit.INTx7=1;
IER|=M_INT1;
EINT;
ERTM;

}
interrupt void ISRTimer0(void)
{
AA++;
CpuTimer0Regs.TCR.bit.TIF=1;
PieCtrlRegs.PIEACK.bit.ACK1=1;
EINT;
}