This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

程序从Flash_to_RAM后无法运行

Other Parts Discussed in Thread: CONTROLSUITE

MCU为F28069,采用Flash_to_RAM的方法,把所有程序都从FLASH移到RAM中运行,但程序运行后无法跳转到main(),不知道什么原因,是因为CMD文件有问题吗?大家帮忙看看。

MEMORY
{
PAGE 0:    /* Program Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
 RAML0_8 : origin = 0x008000, length = 0x00B800    /* on-chip RAM */
    OTP         : origin = 0x3D7800, length = 0x000400     /* on-chip OTP */
    FLASHD_H    : origin = 0x3D8000, length = 0x014000     /* on-chip FLASH */
    FLASHA_C    : origin = 0x3EC000, length = 0x00BF80     //origin = 0x3F0000, length = 0x007F80     /* on-chip FLASH */
    CSM_RSVD    : origin = 0x3F7F80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
    BEGIN_FLASH : origin = 0x3F7FF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
    CSM_PWL     : origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */
    ROM         : origin = 0x3FC000, length = 0x003F00     /* Boot ROM */
   //FPUTABLES   : origin = 0x3FD590, length = 0x000600  /* FPU Tables in Boot ROM */
   //IQTABLES    : origin = 0x3FDC30, length = 0x000B50    /* IQ Math Tables in Boot ROM */
   //IQTABLES2   : origin = 0x3FE780, length = 0x00008C    /* IQ Math Tables in Boot ROM */
   //IQTABLES3   : origin = 0x3FE80C, length = 0x0000AA  /* IQ Math Tables in Boot ROM */

   RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
   VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */
PAGE 1 :   /* Data Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
           /* Registers remain on PAGE1                                                  */
   BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */
   RAMM01       : origin = 0x000050, length = 0x0007B0     /* on-chip RAM block M0 */
   RAML8       : origin = 0x012000, length = 0x001800     /* on-chip RAM block L8. From 0x13800 to 0x14000 is reserved for InstaSPIN */
   USB_RAM     : origin = 0x040000, length = 0x000800     /* USB RAM    */
}
/**************************************************************/
/* Link all user defined sections                             */
/**************************************************************/
SECTIONS
{
/*** Code Security Password Locations ***/
    csmpasswds      : > CSM_PWL,      PAGE = 0  /* Used by file CSMPasswords.asm */
    csm_rsvd        : > CSM_RSVD,     PAGE = 0  /* Used by file CSMPasswords.asm */  
/*** User Defined Sections ***/
    codestart       : > BEGIN_FLASH, PAGE = 0        /* Used by file CodeStartBranch.asm */
    wddisable  : > FLASHA_C,  PAGE = 0  /* Used by file CodeStartBranch.asm */
   copysections : > FLASHA_C,  PAGE = 0  /* Used by file SectionCopy.asm */

 .reset          : > RESET,       PAGE = 0, TYPE = DSECT
 vectors         : > VECTORS,      PAGE = 0, TYPE = DSECT
/*** Uninitialized Sections ***/
    /* Allocate uninitalized data sections: */
    .stack          : > RAMM01,        PAGE = 1
    .ebss           : > RAML8,        PAGE = 1
    .esysmem        : > RAML8,        PAGE = 1
   IQmath              : > FLASHA_C,   PAGE = 0            /* Math Code */
   //IQmathTables        : > IQTABLES,   PAGE = 0, TYPE = NOLOAD
/*** Initialized Sections ***/                                         
   .cinit   : LOAD = FLASHA_C, PAGE = 0 /* Load section to Flash */
                  RUN = RAML0_8,   PAGE = 0    /* Run section from RAM */
                  LOAD_START(_cinit_loadstart),
                  RUN_START(_cinit_runstart),
      SIZE(_cinit_size)
 .const   :   LOAD = FLASHA_C,   PAGE = 0    /* Load section to Flash */
                  RUN = RAML0_8,  PAGE = 0    /* Run section from RAM */
                  LOAD_START(_const_loadstart),
                  RUN_START(_const_runstart),
      SIZE(_const_size)
 .econst   :   LOAD = FLASHA_C,   PAGE = 0    /* Load section to Flash */
                  RUN = RAML0_8,   PAGE = 0    /* Run section from RAM */
                  LOAD_START(_econst_loadstart),
                  RUN_START(_econst_runstart),
      SIZE(_econst_size)

 .pinit   :   LOAD = FLASHA_C,   PAGE = 0    /* Load section to Flash */
                  RUN = RAML0_8,   PAGE = 0    /* Run section from RAM */
                  LOAD_START(_pinit_loadstart),
                  RUN_START(_pinit_runstart),
      SIZE(_pinit_size)
 .switch   :   LOAD = FLASHA_C,   PAGE = 0    /* Load section to Flash */
                  RUN = RAML0_8,   PAGE = 0    /* Run section from RAM */
                  LOAD_START(_switch_loadstart),
                  RUN_START(_switch_runstart),
      SIZE(_switch_size)
 .text   :   LOAD = FLASHA_C,  PAGE = 0    /* Load section to Flash */
                  RUN = RAML0_8,   PAGE = 0    /* Run section from RAM */
                  LOAD_START(_text_loadstart),
                  RUN_START(_text_runstart),
      SIZE(_text_size)
}
/******************* end of file ************************/