This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问在用ccsv8导入很早之前版本的工程的时候出现以下报错,怎么解决 ?



Description Resource Path Location Type
This project was created using a version of compiler that is not currently installed - 5.2.6 [C2000]. See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update. Visit <a href="liveaction:OpenAppCenter">CCS App Center</a> to get the latest compiler support. Or <a href="software-dl.ti.com/.../a> and install the compiler, then register it with CCS through 'Preferences > CCS > Build > Compilers'. DSP28335_PMSM_MAGEncoderV16_2 properties Problem

已经安踏说的升级了代码生成器,还是没有效果。

谢谢