This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28377D采样时间过长,请问有可能是什么原因?

Other Parts Discussed in Thread: CONTROLSUITE

问题描述:F28377D采样时间过长。

实验条件与结果:ADCD进行D0,D1和D2采样,时钟200MHz,ADCCTL2.PRESCALE = 6,程序运行正确,采样结果正确。

补充:如果在中断里利用ADCINT1的标志位来判断采样是否结束,采样时间约190us;

           如果在中断里利用ADCCTL1. ADCBSY来判断采样是否结束,采样时间不超过20us。

请问产生以上情况的原因有可能是什么?

  • ”实验条件与结果:ADCD进行D0,D1和D2采样,时钟200MHz,ADCCTL2.PRESCALE = 6,程序运行正确,采样结果正确。

    补充:如果在中断里利用ADCINT1的标志位来判断采样是否结束,采样时间约190us;

    如果在中断里利用ADCCTL1. ADCBSY来判断采样是否结束,采样时间不超过20us。

    请问产生以上情况的原因有可能是什么?“
    Eric:
    我觉得有可能是判断或测量方法上出问题了。 正常的ADC采样不可能需要那么长的时间。你可以用例程测试一下。另外,看看采样保持时间。
    C:\ti\controlSUITE\device_support\F2837xD\v210\F2837xD_examples_Cpu1\adc_soc_epwm