This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI例程F28027 for PSFB中PWM和comparator配置问题



Hi all

TI 2802x PSFB PCMC里关于PWM初始化配置有个地方不懂,PWM3作为PWM2、4的bypass sync讯号,

其配置的位移量35对于整体控制有甚么作用吗?  对于ADC、COMP1是否有时序上的影响?

另外,在PWM起始时,比较器对于PWM2的动作是如何,能不能稍微解释一下,谢谢。

//Configure EPWM(n+2) time base for ADC SOC generation and syncing the DAC

//Time Base SubModule Register
(*ePWM[n + 2]).TBCTL.bit.PRDLD = TB_IMMEDIATE;
(*ePWM[n + 2]).TBPRD = period - 1;
(*ePWM[n + 2]).TBPHS.half.TBPHS = period - 35;
(*ePWM[n + 2]).TBCTR = 0;

  • "TI 2802x PSFB PCMC里关于PWM初始化配置有个地方不懂,PWM3作为PWM2、4的bypass sync讯号,

    其配置的位移量35对于整体控制有甚么作用吗? 对于ADC、COMP1是否有时序上的影响?

    另外,在PWM起始时,比较器对于PWM2的动作是如何,能不能稍微解释一下,谢谢。"
    ERIC:
    这里的-35就是同步信号来的时候,其他的PWM和前面的PWM之间的相位差。产生移相的效果。对ADC或COMP1应该是没影响,主要看ADC的触发信号是不是由最前面的PWM触发的。