This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tms320f28075 利用FAPI函数烧写Flash无法Boot进入Flash运行

代码通过CCS7.3烧写后,复位或断电运行正常,通过编写的SCI-BootLoader 代码调用FAPI函数将程序写入Flash,校验成功,也可以观察到代码被正确写入,但复位或掉电后,无法运行程序,通过CCS可以看到Boot过程停止到“estop”代码,没有进入0x80000入口执行code-branch代码,GPIO72和GPIO84Boot引脚为高电平。why?难道还需要编程OTP?

  • 请参考手册第三章与BOOT设置相关的内容。

    GPIO72/84处于高电平时系统处于GET MODE模式, 可以观察一下OTP此时是否设置为了Flash Boot模式。