This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

为什么28027的spi自测程序一点没反应



为什么28027的spi自测程序一点没反应,而且程序就停留在了while(SPI_getRxFifoStatus(mySpi) == SPI_FifoStatus_Empty){
             }这一句,好奇怪还是c2000自带的自测程序啊

#include "DSP28x_Project.h"     // Device Headerfile and Examples Include Files
////////////////////////////////////////////////////////////////////////////////
#include "f2802x_common/include/clk.h"
#include "f2802x_common/include/flash.h"
#include "f2802x_common/include/gpio.h"
#include "f2802x_common/include/pie.h"
#include "f2802x_common/include/pll.h"
#include "f2802x_common/include/wdog.h"
#include "f2802x_common/include/spi.h"
//#include "f2802x_common/include/pie_init.h"
////////////////////////////////////////////
void Gpio_setup(void);
void Spi_setup(void);
void Spi_init(void);
void Spi_fifo_init(void);
/////////////////////////
//全局变量
uint16_t count;
uint16_t flag;
////////////////////////
ADC_Handle myAdc;
CLK_Handle myClk;
FLASH_Handle myFlash;
GPIO_Handle myGpio;
PIE_Handle myPie;
SPI_Handle mySpi;
/////////////////////////
void main(void)
{
    uint16_t sdata;  // send data
    uint16_t rdata;  // received data
    CPU_Handle myCpu;
    PLL_Handle myPll;
    WDOG_Handle myWDog;
    // Initialize all the handles needed for this application
    myAdc = ADC_init((void *)ADC_BASE_ADDR, sizeof(ADC_Obj));
    myClk = CLK_init((void *)CLK_BASE_ADDR, sizeof(CLK_Obj));
    myCpu = CPU_init((void *)NULL, sizeof(CPU_Obj));
    myFlash = FLASH_init((void *)FLASH_BASE_ADDR, sizeof(FLASH_Obj));
    myGpio = GPIO_init((void *)GPIO_BASE_ADDR, sizeof(GPIO_Obj));
    myPie = PIE_init((void *)PIE_BASE_ADDR, sizeof(PIE_Obj));
    myPll = PLL_init((void *)PLL_BASE_ADDR, sizeof(PLL_Obj));
    mySpi = SPI_init((void *)SPIA_BASE_ADDR, sizeof(SPI_Obj));
    myWDog = WDOG_init((void *)WDOG_BASE_ADDR, sizeof(WDOG_Obj));

    // Perform basic system initialization
    WDOG_disable(myWDog);
    CLK_enableAdcClock(myClk);
    (*Device_cal)();

    //Select the internal oscillator 1 as the clock source
    CLK_setOscSrc(myClk, CLK_OscSrc_Internal);

    // Setup the PLL for x10 /2 which will yield 50Mhz = 10Mhz * 10 / 2
    PLL_setup(myPll, PLL_Multiplier_10, PLL_DivideSelect_ClkIn_by_2);

    // Disable the PIE and all interrupts
    PIE_disable(myPie);
    PIE_disableAllInts(myPie);
    CPU_disableGlobalInts(myCpu);
    CPU_clearIntFlags(myCpu);
    Gpio_setup();
    Spi_setup();
    PIE_enable(myPie);
    Spi_fifo_init();
    Spi_init ();

    sdata = 0x0000;
/////////////////////////////////////////////
//主循环
    while(1)
    {
            // Transmit data
             SPI_write(mySpi, sdata);
             // Wait until data is received

             while(SPI_getRxFifoStatus(mySpi) == SPI_FifoStatus_Empty){
             }
             // Check against sent data
             rdata = SPI_read(mySpi);
                if(rdata != sdata)  {GPIO_setLow(myGpio, GPIO_Number_2);GPIO_setHigh(myGpio, GPIO_Number_3);}
                else                {GPIO_setLow(myGpio, GPIO_Number_3);GPIO_setHigh(myGpio, GPIO_Number_2);}
                sdata++;
             DELAY_US(1000000);
    }
}
/////////////////////////////////////////////
void Gpio_setup(void)
{
    GPIO_setPullUp(myGpio, GPIO_Number_2, GPIO_PullUp_Disable);
    GPIO_setMode(myGpio, GPIO_Number_2,  GPIO_0_Mode_GeneralPurpose);
    GPIO_setDirection(myGpio, GPIO_Number_2, GPIO_Direction_Output);
    GPIO_setPullUp(myGpio, GPIO_Number_3, GPIO_PullUp_Disable);
    GPIO_setMode(myGpio, GPIO_Number_3,  GPIO_0_Mode_GeneralPurpose);
    GPIO_setDirection(myGpio, GPIO_Number_3, GPIO_Direction_Output);
}
//////////////////////////////////////////////////////////////
void Spi_setup(void)
{
    //初始化外设接口上拉电阻使能
    GPIO_setPullUp(myGpio, GPIO_Number_16, GPIO_PullUp_Enable);
    GPIO_setPullUp(myGpio, GPIO_Number_17, GPIO_PullUp_Enable);
    GPIO_setPullUp(myGpio, GPIO_Number_18, GPIO_PullUp_Enable);
    GPIO_setPullUp(myGpio, GPIO_Number_19, GPIO_PullUp_Enable);
    //异步输入,不校验
    GPIO_setQualification(myGpio, GPIO_Number_16, GPIO_Qual_ASync);
    GPIO_setQualification(myGpio, GPIO_Number_17, GPIO_Qual_ASync);
    GPIO_setQualification(myGpio, GPIO_Number_18, GPIO_Qual_ASync);
    GPIO_setQualification(myGpio, GPIO_Number_19, GPIO_Qual_ASync);
    //设置为SPI总线功能的模式
    GPIO_setMode(myGpio, GPIO_Number_16, GPIO_16_Mode_SPISIMOA);
    GPIO_setMode(myGpio, GPIO_Number_17, GPIO_17_Mode_SPISOMIA);
    GPIO_setMode(myGpio, GPIO_Number_18, GPIO_18_Mode_SPICLKA);
    GPIO_setMode(myGpio, GPIO_Number_19, GPIO_19_Mode_SPISTEA_NOT);
}
//////////////////
void Spi_init(void)
{
 /*//开启spi时钟
 CLK_enableSpiaClock(myClk);
    //***-***-0复位spi外设,上升沿输入数据,设置8位长度
    SPI_setCharLength(mySpi, SPI_CharLength_8_Bits);
    //***-master/slave使能主机,正常spi时钟方式
    SPI_setMode(mySpi, SPI_Mode_Master);
    //***-talk发送时能,关闭spi中断
    SPI_enableTx(mySpi);
    //SPIBRR使能波特率500K
    SPI_setBaudRate(mySpi, SPI_BaudRate_500_KBaud);
    //用于内部自测SPICCR-spilbk
    SPI_enableLoopBack(mySpi);
    //从复位中恢复SPICCR-spi sw reset
    SPI_enable(mySpi);//为什么这个函数没有原型
    //自由运行忽视中断挂起
    SPI_setPriority(mySpi, SPI_Priority_FreeRun);//SPIPRI-spi susp soft/free*/
    CLK_enableSpiaClock(myClk);

    // Reset on, rising edge, 16-bit char bits
    SPI_setCharLength(mySpi, SPI_CharLength_16_Bits);

    // Enable master mode, normal phase,
    // enable talk, and SPI int disabled.
    SPI_setMode(mySpi, SPI_Mode_Master);
    SPI_enableTx(mySpi);

    SPI_setBaudRate(mySpi, SPI_BaudRate_1_MBaud);

    // Relinquish SPI from Reset
    SPI_enableLoopBack(mySpi);
    SPI_enable(mySpi);

    // Set so breakpoints don't disturb xmission
    SPI_setPriority(mySpi, SPI_Priority_FreeRun);
}
///////////////////////////
void Spi_fifo_init(void)
{
    /*//初始化SPI FIFO 寄存器
 //SPIRST使能发送和接收通道
    SPI_enableChannels(mySpi);
    //SPIFFENA使能spi fifo寄存器使能
    SPI_enableFifoEnh(mySpi);
    //TXFIFO Reset复位先写0再置位
    SPI_resetTxFifo(mySpi);
    //TXFFINT CLR清除TXFFINT中断标志
    SPI_clearTxFifoInt(mySpi);
    //默认是TXFFIENA=0不匹配
    ///////////////////////////////
    //RXFIFO Reset写0再写1复位
    SPI_resetRxFifo(mySpi);
    //RXFFINT CLR清除RXFFINT中断标志
    SPI_clearRxFifoInt(mySpi);
    //设置RX的深度为4级
    SPI_setRxFifoIntLevel(mySpi, SPI_FifoLevel_4_Words);
    //RXfifo在接受数据大于4时中断标志置位
    //TXfifo在发送数据小于等于0时才置位
    //设定fifo写延时
    SPI_setTxDelay(mySpi,10);*/
 // Initialize SPI FIFO registers
     SPI_enableChannels(mySpi);
     SPI_enableFifoEnh(mySpi);
     SPI_clearTxFifoInt(mySpi);
     SPI_clearRxFifoInt(mySpi);
     SPI_resetRxFifo(mySpi);
     SPI_resetTxFifo(mySpi);
     SPI_setRxFifoIntLevel(mySpi, SPI_FifoLevel_4_Words);
}