This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28027F无感FOC限制输入功率,控制电流,转速问题



问题描述:

1、目前采用28027F无感foc控制压缩机,假设我设定转速3000,正常工况下输入功率1000W,因为比如外部散热等问题,导致负载增大,如果要维持3000转速,必然导致输入功率增大。我希望输入功率限制在一定范围,所以目前采用FOC内部的Iq_A,或者Is_A来进行限制,比如当Is_A超过一个值时,就在当前转速降低下降低200转,当下降到一定值时,再升速。目前感觉这种方案有时可以,有时会失效。。。

请问各位热心人,这种靠IS_A来的值来限制转速,进而保证输入功率不超是否可行?

2、第二种方案,我在直流母线上串入一个0.02采样电阻,经过预算放大器放大后进入AD,准备通过采集母线上的电流来限制。有个问题是母线上电流也是波动的,怎么获得电流平均值?是通过低通滤波器后进入AD后采集多次进行平均?那采样点怎么设计?

谢谢各位!