This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dsp28035 ADC



dsp2812的ADC中有最大转换通道寄存器,而dsp28035中没有,当我只想采样3个通道时,dsp28035怎么设置呢?而且它的寄存器的默认值大多为0,如果不设置,也不符合我的期望。

  • 每一路的SOC可以自由选择采样通道    以前的可能排好序后顺序去转换 

  • SOC可以理解为一个内部事件,这个事件决定了转换和采样的优先级,而这个事件可以独立配置到任意外部ADC引脚,以及配置自己的采样窗宽度,和被触发采样的触发源。所以会相对F28335的顺序触发采样灵活,也就是您可以理解为每个采样通道都可以通过SOC的配置变成任意优先级。并且通过不同的触发源配置可以控制不同的采样周期。

    e2echina.ti.com/.../114875

    您可以设置 AdcRegs.ADCSOCxCTL.bit.CHSEL
  • AdcRegs.ADCSOCxCTL.bit.CHSEL的默认值是0,现在我只想采样3个通道,AdcRegs.ADCSOC0CTL.bit.CHSEL = 0;AdcRegs.ADCSOC1CTL.bit.CHSEL = 1;AdcRegs.ADCSOC2CTL.bit.CHSEL =2;那其他AdcRegs.ADCSOCxCTL.bit.CHSEL是0,是不是也不适合?

    我做了一个实验,通道选择,我只写了两句话,ADCSOC0CTL ADCSOC1CTL分别选了ADCINA0和ADCINA1,查看ADC结果寄存器,发现ADCRESULT0和ADCRESULT1有数据,其它的结果寄存器全是0,其它通道应该没有转换。但是还是不明白为什么?
  • 只想采样3个通道,您就只需设置 AdcRegs.ADCSOC0CTL.bit.CHSEL = 0;AdcRegs.ADCSOC1CTL.bit.CHSEL = 1;AdcRegs.ADCSOC2CTL.bit.CHSEL =2;那其他AdcRegs.ADCSOCxCTL.bit.CHSEL不需要您再去设置

    关于您的实验,能给出详细代码吗?
  • // Configure ADC
    EALLOW;
    AdcRegs.ADCCTL1.bit.INTPULSEPOS = 1; //ADCINT1 trips after AdcResults latch;1 在转换结束产生中断 0 在转换开始产生中断
    AdcRegs.INTSEL1N2.bit.INT1E = 1; //Enabled ADCINT1 触发cla task
    AdcRegs.INTSEL1N2.bit.INT1CONT = 0; //Disable ADCINT1 Continuous mode
    AdcRegs.INTSEL1N2.bit.INT1SEL = 0x01; //setup EOC1 to trigger ADCINT1 to fire

    AdcRegs.ADCSOC0CTL.bit.CHSEL = 0; //set SOC0 channel select to ADCINA0
    AdcRegs.ADCSOC1CTL.bit.CHSEL = 1; //set SOC1 channel select to ADCINA1
    /* AdcRegs.ADCSOC2CTL.bit.CHSEL = 2; //set SOC2 channel select to ADCINA2
    AdcRegs.ADCSOC3CTL.bit.CHSEL = 3; //set SOC3 channel select to ADCINA3
    AdcRegs.ADCSOC4CTL.bit.CHSEL = 4; //set SOC4 channel select to ADCINA4
    AdcRegs.ADCSOC5CTL.bit.CHSEL = 5; //set SOC5 channel select to ADCINA5
    AdcRegs.ADCSOC6CTL.bit.CHSEL = 6; //set SOC6 channel select to ADCINA6
    AdcRegs.ADCSOC7CTL.bit.CHSEL = 7; //set SOC7 channel select to ADCINA7
    AdcRegs.ADCSOC8CTL.bit.CHSEL = 8; //set SOC8 channel select to ADCINB0
    AdcRegs.ADCSOC9CTL.bit.CHSEL = 9; //set SOC9 channel select to ADCINB1
    AdcRegs.ADCSOC10CTL.bit.CHSEL = 10; //set SOC10 channel select to ADCINB2
    AdcRegs.ADCSOC11CTL.bit.CHSEL = 11; //set SOC11 channel select to ADCINB3
    AdcRegs.ADCSOC12CTL.bit.CHSEL = 12; //set SOC12 channel select to ADCINB4
    AdcRegs.ADCSOC13CTL.bit.CHSEL = 13; //set SOC13 channel select to ADCINB5
    AdcRegs.ADCSOC14CTL.bit.CHSEL = 14; //set SOC14 channel select to ADCINB6
    AdcRegs.ADCSOC15CTL.bit.CHSEL = 15; //set SOC15 channel select to ADCINB7
    */
    AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 0x0B; //set ePWM4, ADCSOCA as the trigger source
    AdcRegs.ADCSOC1CTL.bit.TRIGSEL = 0x0B;
    /* AdcRegs.ADCSOC2CTL.bit.TRIGSEL = 5;
    AdcRegs.ADCSOC3CTL.bit.TRIGSEL = 5;
    AdcRegs.ADCSOC4CTL.bit.TRIGSEL = 5;
    AdcRegs.ADCSOC5CTL.bit.TRIGSEL = 5;
    AdcRegs.ADCSOC6CTL.bit.TRIGSEL = 5;
    AdcRegs.ADCSOC7CTL.bit.TRIGSEL = 5;
    AdcRegs.ADCSOC8CTL.bit.TRIGSEL = 5;
    AdcRegs.ADCSOC9CTL.bit.TRIGSEL = 5;
    AdcRegs.ADCSOC10CTL.bit.TRIGSEL = 5;
    AdcRegs.ADCSOC11CTL.bit.TRIGSEL = 5;
    AdcRegs.ADCSOC12CTL.bit.TRIGSEL = 5;
    AdcRegs.ADCSOC13CTL.bit.TRIGSEL = 5;
    AdcRegs.ADCSOC14CTL.bit.TRIGSEL = 5;
    AdcRegs.ADCSOC15CTL.bit.TRIGSEL = 5;
    */
    AdcRegs.ADCSOC0CTL.bit.ACQPS = 9; //set SOC0 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
    AdcRegs.ADCSOC1CTL.bit.ACQPS = 9; //set SOC1 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
    /* AdcRegs.ADCSOC2CTL.bit.ACQPS = 9; //set SOC2 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
    AdcRegs.ADCSOC3CTL.bit.ACQPS = 9; //set SOC3 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
    AdcRegs.ADCSOC4CTL.bit.ACQPS = 9; //set SOC4 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
    AdcRegs.ADCSOC5CTL.bit.ACQPS = 9; //set SOC5 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
    AdcRegs.ADCSOC6CTL.bit.ACQPS = 9; //set SOC6 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
    AdcRegs.ADCSOC7CTL.bit.ACQPS = 9; //set SOC7 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
    AdcRegs.ADCSOC8CTL.bit.ACQPS = 9; //set SOC8 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
    AdcRegs.ADCSOC9CTL.bit.ACQPS = 9; //set SOC9 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
    AdcRegs.ADCSOC10CTL.bit.ACQPS = 9; //set SOC10 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
    AdcRegs.ADCSOC11CTL.bit.ACQPS = 9; //set SOC11 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
    AdcRegs.ADCSOC12CTL.bit.ACQPS = 9; //set SOC12 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
    AdcRegs.ADCSOC13CTL.bit.ACQPS = 9; //set SOC13 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
    AdcRegs.ADCSOC14CTL.bit.ACQPS = 9; //set SOC14 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
    AdcRegs.ADCSOC15CTL.bit.ACQPS = 9; //set SOC15 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
    */
    AdcRegs.ADCINTSOCSEL1.bit.SOC0 = 0; //No ADCINT will trigger SOCx. TRIGSEL field determines SOCx trigger.
    AdcRegs.ADCINTSOCSEL1.bit.SOC1 = 0;
    AdcRegs.ADCINTSOCSEL1.bit.SOC2 = 0;
    AdcRegs.ADCINTSOCSEL1.bit.SOC3 = 0;
    AdcRegs.ADCINTSOCSEL1.bit.SOC4 = 0;
    AdcRegs.ADCINTSOCSEL1.bit.SOC5 = 0;
    AdcRegs.ADCINTSOCSEL1.bit.SOC6 = 0;
    AdcRegs.ADCINTSOCSEL1.bit.SOC7 = 0;
    AdcRegs.ADCINTSOCSEL2.bit.SOC8 = 0;
    AdcRegs.ADCINTSOCSEL2.bit.SOC9 = 0;
    AdcRegs.ADCINTSOCSEL2.bit.SOC10 = 0;
    AdcRegs.ADCINTSOCSEL2.bit.SOC11 = 0;
    AdcRegs.ADCINTSOCSEL2.bit.SOC12 = 0;
    AdcRegs.ADCINTSOCSEL2.bit.SOC13 = 0;
    AdcRegs.ADCINTSOCSEL2.bit.SOC14 = 0;
    AdcRegs.ADCINTSOCSEL2.bit.SOC15 = 0;
    EDIS;