This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

基于dsp28027 SPI模块8位FIFO自测续



前面说到28027的spi模块进行16位数据的传输的时候可以完全按照要求,但是在8位数据传送的时候却遇到了问题一直不能正确的进行校验,后同房过检查发现一方面是点自己的语法错误 sdata = stata <<8; rdata 能正确的接收到(sdata<<8)数据,此时sdata的数值不再是sdata而是(sdata<<8)导致(rdata&0x00ff)一直不等于sdata,今天很高兴找出这个错误,低级错误.以下是我的程序

#include"DSP28x_Project.h"
void gpiosetup(void);
void spisetup(void);
/////////////////////////
void main(void)
{
  uint16_t count;
  uint16_t rdata=0;
  uint16_t sdata=0x0000;
  InitSysCtrl();
  DINT;//关中断
  IER = 0x0000;
  IFR = 0x0000;
  //初始化PIE
  InitPieCtrl();
  //初始化PIE中断向量
  InitPieVectTable();
  ///////////////////
  gpiosetup();
  spisetup();
  while(1)
  {
   sdata = count;
   SpiaRegs.SPITXBUF=(sdata<<8);
   while(SpiaRegs.SPIFFRX.bit.RXFFST!=1){}
   //while(SpiaRegs.SPISTS.bit.INT_FLAG ==0){}
   rdata = SpiaRegs.SPIRXBUF;
   rdata &= 0x00ff;
   if(rdata!=sdata) GpioDataRegs.GPACLEAR.bit.GPIO3 = 1 ;
   else                      GpioDataRegs.GPASET.bit.GPIO3 = 1 ;
   if(count%2)       GpioDataRegs.GPACLEAR.bit.GPIO2 = 1 ;
   else              GpioDataRegs.GPASET.bit.GPIO2 = 1 ;
      DELAY_US(500000);
      if(++count>250)count=0;
  }
}
void gpiosetup(void)
{
 EALLOW;//去保护
 ///功能选择
 //GPIO通用引脚
 GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 0;
 GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 0;
 //SPI模式引脚
 GpioCtrlRegs.GPAMUX2.bit.GPIO16 = 1;
 GpioCtrlRegs.GPAMUX2.bit.GPIO17 = 1;
 GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 1;
 GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 1;
    ///////输出
 GpioCtrlRegs.GPADIR.bit.GPIO2 = 1;
 GpioCtrlRegs.GPADIR.bit.GPIO3 = 1;
 //SPI输入
 GpioCtrlRegs.GPADIR.bit.GPIO16 = 0;
 GpioCtrlRegs.GPADIR.bit.GPIO17 = 0;
 GpioCtrlRegs.GPADIR.bit.GPIO18 = 0;
 GpioCtrlRegs.GPADIR.bit.GPIO19 = 0;
 //输入校验周期QUALPRD2=0默认为0
 //输入校验次数为异步输入
 GpioCtrlRegs.GPAQSEL2.bit.GPIO16=3;
 GpioCtrlRegs.GPAQSEL2.bit.GPIO17=3;
 GpioCtrlRegs.GPAQSEL2.bit.GPIO18=3;
 GpioCtrlRegs.GPAQSEL2.bit.GPIO19=3;
 //上拉电阻使能
 GpioCtrlRegs.GPAPUD.bit.GPIO2 =1;
 GpioCtrlRegs.GPAPUD.bit.GPIO3 =1;
 GpioCtrlRegs.GPAPUD.bit.GPIO16 =1;
 GpioCtrlRegs.GPAPUD.bit.GPIO17 =1;
 GpioCtrlRegs.GPAPUD.bit.GPIO18 =1;
 GpioCtrlRegs.GPAPUD.bit.GPIO19 =1;
 EDIS;//写保护
}
void spisetup(void)
{
 //Sip时钟已开启60M/4
 //软件复位spi
 SpiaRegs.***.bit.SPISWRESET = 0;
 //spi不工作时候spiclk保持高电平
 SpiaRegs.***.bit.CLKPOLARITY = 0;
 //允许spi内部自测功能
 SpiaRegs.***.bit.SPILBK = 1;
 //8位数据模式
 SpiaRegs.***.bit.*** = 7;
    //相位极性是上降沿所存数据下降沿发送数据
 SpiaRegs.***.bit.CLK_PHASE = 0;
 //主机模式
 SpiaRegs.***.bit.MASTER_SLAVE = 1;
 //允许发送功能
 SpiaRegs.***.bit.TALK = 1;
 //60M/4/(1+99)=150K
 SpiaRegs.SPIBRR = 99;

 //使能FIFO发送操作
 SpiaRegs.SPIFFTX.bit.TXFIFO= 0;
 SpiaRegs.SPIFFTX.bit.SPIFFENA = 1;
 SpiaRegs.SPIFFTX.bit.TXFFIL = 0;
 SpiaRegs.SPIFFTX.bit.TXFFIENA= 0;
 SpiaRegs.SPIFFTX.bit.TXFFINTCLR = 1;
 //使能FIFO接收操作
 SpiaRegs.SPIFFRX.bit.RXFIFORESET= 0;
 SpiaRegs.SPIFFRX.bit.RXFFIENA = 0;
 SpiaRegs.SPIFFRX.bit.RXFFIL = 4;
 SpiaRegs.SPIFFRX.bit.RXFFINTCLR = 1;
 //0延时
 SpiaRegs.SPIFFCT.all = 0;
 //
 SpiaRegs.SPIPRI.bit.FREE = 1;
 //退出复位进入工作状态
 SpiaRegs.SPIFFTX.bit.TXFIFO = 1;
 SpiaRegs.SPIFFRX.bit.RXFIFORESET = 1;/**/
 SpiaRegs.SPISTS.all = 0x00;
 SpiaRegs.***.bit.SPISWRESET = 1;
 //重新开始FIFO的接收或者发送操作
 SpiaRegs.SPIFFTX.bit.SPIRST= 1;//


}

http://hi.baidu.com/nizhenyu/item/8b261336cdc02c83f4e4ad38