This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助



我在编译: 377S时,出现如下:

warning #10247-D: creating output section "ramfuncs" without a SECTIONS specification
"../28377S_FLASH_lnk.cmd", line 111: error #10099-D: program will not fit into available memory. run placement with alignment/blocking fails for section ".ebss" size 0x50fb page 1. Available memory ranges:
RAMLS5 size: 0x800 unused: 0x21c max hole: 0x21b
RAMGS0 size: 0x1000 unused: 0xc40 max hole: 0xc40
RAMGS1 size: 0x1000 unused: 0x1000 max hole: 0x1000
error #10010: errors encountered during linking; "ADC_SOC_DIFF.out" not built

该如何解决?  

可能的原因是我在某一个文件中定义了一个大小为 20000byte 的数组,  但我的项目要求就需要更大的数组。